MCUXpresso SDK Documentation

Run a demo application using Arm GCC

Run a demo application using Arm GCC#

This document uses peripheral_ht example to describe the steps to open a project, build an example, and run a project on MDK.

For details, see the related section in Getting Started with MCUXpresso SDK User’s Guide (document: MCUXSDKGSUG) at root/docs/ and the readme file in the corresponding demo’s directory.

Setup tool chains#

See the section “Run a demo using Arm GCC” of getting start document. For example, Getting Started with MCUXpresso SDK for MIMXRT1170-EVKB.

Parent topic:Run a demo application using Arm GCC

Build a GCC example#

To build a GCC example:

  1. Change the directory to the project directory: <install_dir>\boards\evkbmimxrt1170\edgefast_open_examples\peripheral_ht\armgcc.

  2. Run the build script.

    For windows, the script is build_flexspi_nor_debug.bat/ build_flexspi_nor_release.bat.

    The build output is shown in the following figure.

Parent topic:Run a demo application using Arm GCC

Run a GCC example#

Refer to the section “Run a demo using Arm GCC” of the getting start document. For example, see Getting Started with MCUXpresso SDK for MIMXRT1170-EVKB. The peripheral_ht.elf is the target to download.

Parent topic:Run a demo application using Arm GCC

Parent topic:Demo