PyTorch Model Conversion to ExecuTorch Format
In this guideline we will show how to use the ExecuTorch AoT part to convert a PyTorch model to ExecuTorch format and delegate the model computation to eIQ Neutron NPU using the eIQ Neutron Backend.
First we will start with an example script converting the model. This example show the CifarNet model preparation. It is the same model which is part of the example_cifarnet
The steps are expected to be executed from the executorch root folder, in our case the mcuxsdk-middleware-executorch
After building the ExecuTorch you shall have the
libquantized_ops_aot_lib.solocated in thepip-outfolder. We will need this library when generating the quantized cifarnet ExecuTorch model. So as first step we will find it:
$ find ./pip-out -name 'libquantized_ops_aot_lib.so'
./pip-out/temp.linux-x86_64-cpython-310/cmake-out/kernels/quantized/libquantized_ops_aot_lib.so
./pip-out/lib.linux-x86_64-cpython-310/executorch/kernels/quantized/libquantized_ops_aot_lib.so
Now run the
aot_neutron_compile.pyexample with thecifar10model
$ python examples/nxp/aot_neutron_compile.py \
--quantize --so_library ./pip-out/lib.linux-x86_64-cpython-310/executorch/kernels/quantized/libquantized_ops_aot_lib.so \
--delegate --neutron_converter_flavor SDK_25_09 -m cifar10
It will generate you
cifar10_nxp_delegate.ptefile which can be used with the MXUXpresso SDKcifarnet_exampleproject.
The generated PTE file is used in the executorch_cifarnet example application, see example_application.