eIQ MCU Media Processing Pipeline API#
MPP VERSION 4.1
1. MPP API#
Functions
int mpp_api_init (mpp_api_params_t ∗params)
mpp_t mpp_create (mpp_params_t ∗params, int ∗ret)
int mpp_camera_add (mpp_t mpp, const char ∗name, mpp_camera_params_t ∗params, mpp_elem_handle_t elem_h)
int mpp_static_img_add (mpp_t mpp, mpp_img_params_t ∗params, void ∗addr)
int mpp_display_add (mpp_t mpp, const char ∗name, mpp_display_params_t ∗params)
int mpp_nullsink_add (mpp_t mpp)
int mpp_element_add (mpp_t mpp, mpp_element_id_t id, mpp_element_params_t ∗params, mpp_elem_handle_t ∗elem_h)
int mpp_split (mpp_t mpp, unsigned int num, mpp_params_t ∗params, mpp_t ∗out_list)
int mpp_background (mpp_t mpp, mpp_params_t ∗params, mpp_t ∗out_mpp)
int mpp_element_update (mpp_t mpp, mpp_elem_handle_t elem_h, mpp_element_params_t ∗params, bool force_update)
int mpp_start (mpp_t mpp, int last)
int mpp_stop (mpp_t mpp)
void mpp_stats_enable (mpp_stats_grp_t grp)
void mpp_stats_disable (mpp_stats_grp_t grp)
char ∗mpp_get_version (void)
bool mpp_is_running (mpp_t mpp)
int mpp_force_update(mpp_t mpp)
1.1 Detailed Description#
This section provides the detailed documentation for the MCU Media Processing Pipeline API.
1.1.1 Function Documentation#
mpp_api_init#
int mpp_api_init ( mpp_api_params_t ∗ params )
Pipeline initialization. This function initializes the library and its data structures. It must be called before any other function of the API is called.
Parameters
in/out |
name |
description |
|---|---|---|
in |
params |
API global parameters |
out |
ret |
return code (0 - success, non-zero - error) |
Returns
mpp_create#
mpp_t mpp_create ( mpp_params_t ∗ params, int ∗ ret )
Basic pipeline creation. This function returns a handle to the pipeline.
Parameters
in/out |
name |
description |
|---|---|---|
in |
params |
pipeline parameters |
out |
ret |
return code (0 - success, non-zero - error) |
Returns
handle to the pipeline if success, NULL if there is an error.
mpp_camera_add#
int mpp_camera_add ( mpp_t mpp, const char ∗ name, mpp_camera_params_t ∗ params, mpp_elem_handle_t elem_h, )
Camera addition.
This function adds a camera to the pipeline.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
input pipeline |
in |
name |
camera driver name |
in |
params |
parameters to be configured on the camera |
out |
elem_h |
element handle in pipeline |
Returns
mpp_static_img_add#
int mpp_static_img_add ( mpp_t mpp, mpp_img_params_t ∗ params, void ∗ addr, mpp_elem_handle_t ∗ elem_h )
Static image addition.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
input pipeline |
in |
params |
static image parameters |
in |
addr |
image buffer |
out |
elem_h |
element handle in pipeline |
Returns
Precondition
Image buffer allocation/free is the responsibility of the user.
mpp_display_add#
int mpp_display_add ( mpp_t mpp, const char ∗ name, mpp_display_params_t ∗ params )
Display addition.
This function adds a display to the pipeline.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
input pipeline |
in |
name |
display driver name |
in |
params |
parameters that are configured on the display |
Returns
mpp_nullsink_add#
int mpp_nullsink_add ( mpp_t mpp )
Null sink addition.
This function adds a null-type sink to the pipeline.
After this call pipeline is closed and no further elements can be added. Input frames are discarded.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
input pipeline |
Returns
mpp_element_add#
int mpp_element_add ( mpp_t mpp, mpp_element_id_t id, mpp_element_params_t ∗ params, mpp_elem_handle_t ∗ elem_h )
Add processing element (single input, single output) This function adds an element to the pipeline. Available elements are:
2D image processing
ML inference engine
Labeled rectangle
Compositor
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
input pipeline |
in |
id |
element id |
in |
params |
element parameters |
out |
elem_h |
element handle in pipeline |
Returns
mpp_split#
int mpp_split ( mpp_t mpp, unsigned int num, mpp_params_t ∗ params, mpp_t ∗ out_list )
Pipeline multiplication.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
input pipeline |
in |
num |
number of output pipeline |
in |
params |
split mpp parameters |
out |
out_list |
list of output pipelines |
Returns
Precondition
out_list array must contain at least num elements.
mpp_background#
int mpp_background ( mpp_t mpp, mpp_params_t ∗ params, mpp_t ∗ out_mpp )
Put next elements processing in background.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
input pipeline |
in |
params |
new mpp parameters (exec_flag must be MPP_EXEC_PREEMPT) |
out |
out_mpp |
output pipeline |
Returns
mpp_element_update#
int mpp_element_update ( mpp_t mpp, mpp_elem_handle_t elem_h, mpp_element_params_t ∗ params, bool force_update )
Update element parameters.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
input pipeline |
in |
elem_h |
element handle in the pipeline. |
in |
params |
new element parameters |
in |
force_update |
force the pipeline to run even though there is no input frame update for processing elements after update. If the force_update flag was already requested before, the current value is ignored |
Returns
mpp_is_running#
bool mpp_is_running ( mpp_tmpp )
Check if the pipeline is currently running
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
input pipeline |
Returns
true if pipeline is in running state, else false
mpp_start#
int mpp_start ( mpp_t mpp, int last )
Start pipeline.
When called with last=0, this function prepares the branch of the pipeline specified with mpp. When called with last!=0, this function starts the data flow of the pipeline.
Data flow should start after all the branches of the pipeline have been prepared.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
pipeline branch handle to start/prepare |
in |
last |
if non-zero start pipeline processing. No further start call is possible thereafter. |
Returns
mpp_stop#
int mpp_stop ( mpp_t mpp )
Stop a branch of the pipeline.
This function stops the data processing and peripherals of a pipeline branch.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
pipeline branch to stop |
Returns
mpp_force_update#
int mpp_force_update ( mpp_t mpp )
Force the update of a branch of the pipeline.
This function forces and update of the branch of the pipeline even if there is no new input frame.
Parameters
in/out |
name |
description |
|---|---|---|
in |
mpp |
pipeline branch to set the flag force_update to true |
Returns
mpp_stats_enable#
void mpp_stats_enable ( mpp_stats_grp_t grp )
Enable statistics collection.
This function enables statistics collection for a given group. Statistics collection is disabled by default after API initialization. Calling this function when stats are enabled has no effect.
Parameters
in/out |
name |
description |
|---|---|---|
in |
grp |
statistics group |
Returns
mpp_stats_disable#
void mpp_stats_disable ( mpp_stats_grp_t grp )
Disable statistics collection.
This function disables statistics collection for a given group. Calling this function when stats are disabled has no effect. This function is used to ensure stats are not updated while application tasks use the stats structures.
Parameters
in/out |
name |
description |
|---|---|---|
in |
grp |
statistics group |
Returns
mpp_get_version#
char ∗ mpp_get_version ( void )
Get MPP version.
Parameters
Returns
pointer to the MPP version string
2. MPP Types#
Data Structures
union mpp_stats_t
struct mpp_api_params_t
struct mpp_params_t
struct mpp_camera_stream_cfg
struct mpp_camera_params_t
struct mpp_img_params_t
struct mpp_display_params_t
struct mpp_tensor_dims_t
struct mpp_inference_cb_param_t
union mpp_color_t
struct mpp_labeled_rect_t
struct mpp_landmark_t
struct mpp_area_t
struct mpp_dims_t
struct mpp_position_t
struct mpp_inference_params_t
struct mpp_element_params_t
struct mpp_stats_t.api
struct mpp_stats_t.mpp
struct mpp_stats_t.elem
struct mpp_color_t.rgb
Macros
#define MPP_INFERENCE_MAX_OUTPUTS
#define MPP_INFERENCE_MAX_INPUTS
#define MPP_INVALID
#define MPP_EVENT_ALL
#define MAX_TENSOR_DIMS
Typedefs
typedef void ∗mpp_t
typedef uintptr_t mpp_elem_handle_t
typedef unsigned int mpp_evt_mask_t
typedef int(∗inference_entry_point_t) (uint8_t ∗, uint8_t ∗, uint8_t ∗)
Enumerations
enum mpp_evt_t {
MPP_EVENT_INFERENCE_OUTPUT_READY,
MPP_EVENT_QUALITY_CHECK_READY,
enum mpp_exec_flag_t {
enum mpp_stats_grp_t {
enum mpp_rotate_degree_t {
enum mpp_flip_mode_t {
enum mpp_convert_ops_t {
enum mpp_pixel_format_t {
enum mpp_element_id_t {
MPP_ELEMENT_LABELED_RECTANGLE,
enum mpp_tensor_type_t {
enum mpp_tensor_order_t {
enum mpp_inference_type_t {
enum mpp_camera_stream_type {
2.1 Detailed Description#
This section provides the detailed documentation for the MCU Media Processing Pipeline types.
2.1.1 Data Structure Documentation#
mpp_stats_t#
union mpp_stats_t
Data Fields
type |
name |
description |
|---|---|---|
struct mpp_stats_t.api |
api |
Global execution performance counters. |
struct mpp_stats_t.mpp |
mpp |
Pipeline execution performance counters. |
struct mpp_stats_t.elem |
elem |
Element execution performance counters. |
mpp_api_params_t#
struct mpp_api_params_t
Data Fields
type |
name |
description |
|---|---|---|
stats |
API stats. |
|
unsigned int |
rc_cycle_min |
minimum cycle duration for RC tasks (ms), 0: sets default value |
unsigned int |
rc_cycle_inc |
time increment for RC tasks (ms), 0: sets default value |
int |
pipeline_task_max_prio |
pipeline tasks maximum priority. |
int |
pipeline_rc_task_prio |
pipeline run-to-completion tasks priority. 0: sets default value |
int |
pipeline_pr_task_prio |
pipeline preemptable tasks priority. 0: sets default value |
mpp_params_t#
struct mpp_params_t
Pipeline creation parameters.
Data Fields
int(∗evt_callback_f )(mpp_t mpp, mpp_evt_t evt, void ∗evt_data, void ∗user_data)
mpp_evt_mask_t mask
mpp_exec_flag_t exec_flag
void ∗cb_userdata
mpp_stats_t#
struct mpp_stats_t
Data Fields
mpp_stats_t ∗stats
mpp_camera_stream_cfg#
struct mpp_camera_stream_cfg
Camera stream configuration for multi-stream cameras.
Data Fields
type |
name |
description |
|---|---|---|
type |
Stream type (member of enum mpp_camera_stream_type) |
|
bool |
active |
Stream is active or not. |
int |
height |
|
int |
width |
mpp_camera_params_t#
struct mpp_camera_params_t
Camera parameters.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
buffer height |
int |
width |
buffer width |
format |
pixel format |
|
int |
fps |
frames per second |
bool |
stripe |
stripe mode |
void * |
rpmsg_inst |
pointer to rpmsg instance |
volatile uint16_t * |
mcmgr_event_data |
pointer to mcmgr event data |
uint32_t |
n_streams |
number of total output video streams |
mpp_camera_stream_cfg |
stream[NUM_STREAMS] |
streams configuration |
bool |
in_advance_enqueue |
enable in-advance enqueue mode |
mpp_img_params_t#
struct mpp_img_params_t
Static image parameters.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
buffer height |
int |
width |
buffer width |
format |
pixel format |
|
bool |
stripe |
stripe mode |
int |
compressed_size |
size in bytes for compressed format |
mpp_display_params_t#
struct mpp_display_params_t
Display parameters.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
buffer resolution: setting to 0 will default to panel physical resolution |
int |
width |
buffer resolution: setting to 0 will default to panel physical resolution |
int |
pitch |
buffer resolution: setting to 0 will default to panel physical resolution |
int |
left |
active rect: setting to 0 will default to fullscreen |
int |
top |
active rect: setting to 0 will default to fullscreen |
int |
right |
active rect: setting to 0 will default to fullscreen |
int |
bottom |
active rect: setting to 0 will default to fullscreen |
rotate |
rotate degree |
|
format |
pixel format |
|
bool |
stripe |
stripe mode |
void ∗ |
handle |
pointer to an lvgl image widget |
mpp_tensor_dims_t#
struct mpp_tensor_dims_t
Inference tensor dimensions.
Data Fields
type |
name |
description |
|---|---|---|
uint32_t |
size |
|
uint32_t |
data[[MAX_TENSOR_DIMS]] |
mpp_inference_tensor_params_t#
struct mpp_inference_tensor_params_t
tensor parameters
Data Fields
type |
name |
description |
|---|---|---|
const uint8_t ∗ |
data |
data address |
dims |
tensor data dimensions |
|
type |
tensor data type |
mpp_inference_cb_param_t#
struct mpp_inference_cb_param_t
Inference callback parameters.
Data Fields
type |
name |
description |
|---|---|---|
void ∗ |
user_data |
callback will pass this pointer |
out_tensors[[MPP_INFERENCE_MAX_OUTPUTS]] |
output tensors parameters |
|
int |
inference_time_ms |
inference run time measurement - output to user |
inference_type |
type of the inference |
img_quality_metrics#
struct img_quality_metrics_t
Data Fields
type |
name |
description |
|---|---|---|
int |
brightness |
brightness metric |
int |
contrast |
contrast metric |
mpp_color_t#
union mpp_color_t
mpp color encoding
Data Fields
type |
name |
description |
|---|---|---|
uint32_t |
raw |
Raw color. |
struct mpp_color_t.rgb |
rgb |
rgb color values RGB color |
mpp_labeled_rect_t#
struct mpp_labeled_rect_t
mpp labeled rectangle element structure
Data Fields
type |
name |
description |
|---|---|---|
uint8_t |
label[64] |
label to print |
uint16_t |
clear |
clear rectangle |
uint16_t |
line_width |
rectangle line thickness |
line_color |
rectangle line color |
|
int16_t |
top |
rectangle top position |
int16_t |
left |
rectangle left position |
int16_t |
bottom |
rectangle bottom position |
int16_t |
right |
rectangle right position |
uint16_t |
tag |
labeled rectangle tag |
uint16_t |
reserved |
pad for 32 bits alignment |
bool |
stripe |
stripe mode |
mpp_landmark_t#
struct mpp_landmark_t
mpp landmark structure
Data Fields
type |
name |
description |
|---|---|---|
uint16_t |
clear |
clear landmark |
color |
landmark color |
|
int16_t |
x |
landmark x position |
int16_t |
y |
landmark y position |
uint16_t |
tag |
landmark tag |
bool |
stripe |
stripe mode |
mpp_area_t#
struct mpp_area_t
Image area coordinates.
Data Fields
type |
name |
description |
|---|---|---|
int |
top |
|
int |
left |
|
int |
bottom |
|
int |
right |
mpp_dims_t#
struct mpp_dims_t
Image dimensions.
Data Fields
type |
name |
description |
|---|---|---|
unsigned int |
width |
|
unsigned int |
height |
mpp_position_t#
struct mpp_position_t
Image position.
Data Fields
struct mpp_inference_params_t
Model parameters.
Data Fields
type |
name |
description |
|---|---|---|
uint64_t |
constant_weight_MemSize |
model constant weights memory size |
uint64_t |
mutable_weight_MemSize |
Defines the amount of memory required both input & output data buffers. |
uint64_t |
activations_MemSize |
Size of scratch memory used for intermediate computations needed by the model. |
int |
num_inputs |
model’s number of inputs |
int |
num_outputs |
model’s number of outputs |
uint64_t |
inputs_offsets[MPP_INFERENCE_MAX_INPUTS] |
offset of each input |
uint64_t |
outputs_offsets[MPP_INFERENCE_MAX_OUTPUTS] |
offset ofeach output |
model_entry_point |
function called to perform the inference |
|
model_input_tensors_type |
type of input buffer |
mpp_img_compose_param_t#
struct mpp_img_compose_param_t
Image composition parameters.
Data Fields
type |
name |
description |
|---|---|---|
int |
height |
original image height |
int |
width |
original image width |
format |
pixel format |
|
void ∗ |
buffer |
image buffer address |
dest_area |
area for image in destination |
mpp_element_params_t#
struct mpp_element_params_t
Static image and Processing elements parameters.
Data Fields
type |
name |
description |
|---|---|---|
__unnamed__ |
||
stats |
mpp_stats_tapi#
struct mpp_stats_t.api
Data Fields
type |
name |
description |
|---|---|---|
unsigned int |
rc_cycle |
run-to-completion (RC) cycle duration (ms) |
unsigned int |
rc_cycle_max |
run-to-completion work deadline (ms) |
unsigned int |
pr_slot |
available slot for preemptable (PR) work (ms) |
unsigned int |
pr_rounds |
number of RC cycles required to complete one PR cycle (ms) |
unsigned int |
app_slot |
remaining time for application (ms) |
unsigned int |
cpu_load |
CPU load percentage (%) |
mpp_stats_tmpp#
struct mpp_stats_t.mpp
Data Fields
type |
name |
description |
|---|---|---|
mpp |
||
unsigned int |
mpp_exec_time |
pipeline execution time (ms) |
mpp_stats_telem#
struct mpp_stats_t.elem
Data Fields
type |
name |
description |
|---|---|---|
hnd |
||
unsigned int |
elem_exec_time |
element execution time (ms) |
mpp_color_trgb#
struct mpp_color_t.rgb
rgb color values
Data Fields
type |
name |
description |
|---|---|---|
uint8_t |
R |
Red byte. |
uint8_t |
G |
Green byte. |
uint8_t |
B |
Blue byte. |
uint8_t |
pad |
padding byte |
mpp_element_params_t__unnamed5__#
union mpp_element_params_t.__unnamed5__
Data Fields
type |
name |
description |
|---|---|---|
camera |
Camera element’s parameters |
|
static_image |
Static Image element’s parameters. |
|
compose |
Compose element’s parameters. |
|
struct |
labels |
Labeled Rectangle and Landmarks element parameters. |
convert |
Convert element’s parameters. |
|
struct |
resize |
Resize element’s parameters. |
color_conv |
Color convert element’s parameters. |
|
struct |
rotate |
Rotate element’s parameters. |
struct |
test |
Test element’s parameters. |
struct |
decode |
Decoder element’s parameters. |
ml_inference |
ML inference element’s parameters. |
|
img_quality_check |
Image quality check element’s parameters. |
mpp_element_params_t__unnamed5__static_image#
struct mpp_element_params_t.__unnamed5__.static_image
Static Image element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
img_params |
static image parameters |
|
void ∗ |
img_buffer |
static image buffer address |
mpp_element_params_t__unnamed5__compose#
struct mpp_element_params_t.__unnamed5__.compose
Compose element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
int |
nb_images |
number of images to compose |
mpp_img_params_t |
logo_img_params |
logo image parameters |
image_list |
pointer to array of images to compose |
|
input_area |
area of input stream in destination |
|
out_angle |
output rotation angle |
|
out_flip |
output flip mode |
|
out_format |
output color format |
|
int |
out_width |
output buffer width |
int |
out_height |
output buffer height |
mpp_element_params_t__unnamed5__labels#
struct mpp_element_params_t.__unnamed5__.labels
Labeled Rectangle element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
uint32_t |
max_rect |
maximum number of rectangles |
uint32_t |
detected_rect |
detected rectangles |
rectangles |
array of rectangle data |
|
uint32_t |
max_landmk |
maximum number of landmarks |
uint32_t |
detected_landmk |
detected landmarks |
mpp_landmark_t * |
landmarks |
array of landmark data |
mpp_element_params_t__unnamed5__convert#
struct mpp_element_params_t.__unnamed5__.convert
Convert element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
out_buf |
output buffer dimensions |
|
pixel_format |
new pixel format |
|
angle |
rotation angle |
|
flip |
flip mode |
|
crop |
input crop area |
|
out_window |
output window position |
|
scale |
scaling dimensions |
|
ops |
operation selector mask |
|
const char ∗ |
dev_name |
device name used for graphics |
bool |
stripe_in |
input stripe mode |
bool |
stripe_out |
output stripe mode |
mpp_element_params_t__unnamed5__resize#
struct mpp_element_params_t.__unnamed5__.resize
Resize element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
unsigned int |
width |
|
unsigned int |
height |
mpp_element_params_t__unnamed5__color_conv#
struct mpp_element_params_t.__unnamed5__.color_conv
Color convert element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
mpp_element_params_t__unnamed5__rotate#
struct mpp_element_params_t.__unnamed5__.rotate
Rotate element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
angle |
mpp_element_params_t__unnamed5__test#
struct mpp_element_params_t.__unnamed5__.test
Test element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
_Bool |
inp |
|
unsigned int |
width |
|
unsigned int |
height |
|
format |
mpp_element_params_t__unnamed5__decode#
struct mpp_element_params_t.__unnamed5__.decode
Decoder element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
const char ∗ |
dev_name |
device name used for decoder |
unsigned int |
width |
|
unsigned int |
height |
|
out_format |
mpp_element_params_t__unnamed5__ml_inference#
struct mpp_element_params_t.__unnamed5__.ml_inference
ML inference element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
const void ∗ |
model_data |
pointer to model binary |
type |
inference type |
|
int |
model_size |
model binary size |
float |
model_input_mean |
model ‘mean’ of input values, used for normalization |
float |
model_input_std |
model ‘standard deviation’ of input values, used for normalization |
tensor_order |
model input tensor component order |
|
inference_params |
model specific parameters used by the inference |
mpp_element_params_t__unnamed5__img_quality_check#
struct mpp_element_params_t.__unnamed5__.img_quality_check
Image quality check element’s parameters.
Data Fields
type |
name |
description |
|---|---|---|
_Bool |
disable |
disable quality check |
2.1.2 Macro Definition Documentation#
MPP_INFERENCE_MAX_OUTPUTS
mpp_inference_max_outputs#
#define MPP_INFERENCE_MAX_OUTPUTS
Maximum number of inference inputs and outputs. Maximum number of outputs supported by the pipeline
mpp_inference_max_inputs#
#define MPP_INFERENCE_MAX_INPUTS
Maximum number of inputs supported by the pipeline.
mpp_invalid#
#define MPP_INVALID Invalid pipeline handle.
mpp_event_all#
#define MPP_EVENT_ALL
Bit mask to receive all Events.
max_tensor_dims#
#define MAX_TENSOR_DIMS
Maximum number of dimensions for tensors.
2.1.3 Typedef Documentation#
mpp_t#
typedef void∗ mpp_t Pipeline handle type.
mpp_elem_handle_t#
typedef uintptr_t mpp_elem_handle_t Element handle type.
mpp_evt_mask_t#
typedef unsigned int mpp_evt_mask_t Event mask for pipeline creation.
inference_entry_point_t#
typedef int(∗ inference_entry_point_t) (uint8_t ∗, uint8_t ∗, uint8_t ∗) Bundle inference function type.
2.1.4 Enumeration Type Documentation#
mpp_evt_t#
enum mpp_evt_t
Pipeline generated events.
Enumerator
mpp_exec_flag_t#
enum mpp_exec_flag_t
Execution parameters.
These parameters control the execution of the elements of an mpp.
The “mpps” created using the flag MPP_EXEC_RC are guaranteed to run up to the completion of all processing elements, while not being preempted by other “mpps”.
The “mpps” created using the flag MPP_EXEC_PREEMPT are preempted after a given time interval by “mpps” that will run-to-completion again.
The “mpps” created with the MPP_EXEC_INHERIT flag inherit the same execution flag as the parent(s) in case of split operation.
Note: It is not possible to request run-to-completion execution when spliting preemptable-execution “mpps”.
Enumerator
mpp_stats_grp_t#
enum mpp_stats_grp_t
Enumerator
mpp_rotate_degree_t#
enum mpp_rotate_degree_t
Rotation value.
Enumerator
mpp_flip_mode_t#
enum mpp_flip_mode_t
Flip type.
Enumerator
mpp_convert_ops_t#
enum mpp_convert_ops_t
The convert operations selector flags.
Enumerator
mpp_pixel_format_t#
enum mpp_pixel_format_t
Pixel format.
Enumerator
label |
description |
|---|---|
ARGB 32 bits. |
|
BGRA 32 bits. |
|
RGBA 32 bits. |
|
BGRX 32 bits. |
|
RGBX 32 bits. |
|
RGB 24 bits. |
|
RGB 16 bits. |
|
BGR 24 bits. |
|
gray 3x8 bits |
|
gray 3x8 bits +8 unused bits |
|
gray 8 bits |
|
gray 16 bits |
|
YUVX interleaved 4:4:4. |
|
VYUY interleaved 4:2:2. |
|
UYVY interleaved 4:2:2. |
|
YUYV interleaved 4:2:2. |
|
depth 16 bits |
|
depth 8 bits |
|
YUV planar 4:2:0. |
|
JPEG. |
|
invalid pixel format |
mpp_camera_stream_type#
Camera stream type for multiple stream camera.
Enumerator
mpp_element_id_t#
enum mpp_element_id_t
Processing element ids.
Enumerator
label |
description |
|---|---|
Invalid element. |
|
Image composition - compose a simple GUI: logo and text area with the input stream. |
|
Labeled rectangle - bounding box. |
|
Test inplace element - NOT FOR USE. |
|
Inference engine. |
|
Image conversion: resolution, orientation, color format. |
|
MPP_ELEMENT_IMG_DECODE |
Image decompression: JPEG, PNG. |
Image quality check: brightness, contrast. |
|
DO NOT USE. |
mpp_tensor_type_t#
enum mpp_tensor_type_t
Inference tensor type.
Enumerator
mpp_tensor_order_t#
enum mpp_tensor_order_t
Inference input tensor order.
Enumerator
mpp_inference_type_t#
enum mpp_inference_type_t
Inference type.
Enumerator
3. Return_codes#
return_codes#
Macros
#define MPP_SUCCESS
#define MPP_ERROR
#define MPP_INVALID_ELEM
#define MPP_INVALID_PARAM
#define MPP_ERR_ALLOC_MUTEX
#define MPP_INVALID_MUTEX
#define MPP_MUTEX_TIMEOUT
#define MPP_MUTEX_ERROR
#define MPP_MALLOC_ERROR
3.1 Detailed Description#
MPP APIs return status definitions.
3.1.1 Macro Definition Documentation#
mpp_success#
#define MPP_SUCCESS
Success return code.
mpp_error#
#define MPP_ERROR
A generic error occured.
mpp_invalid_elem#
#define MPP_INVALID_ELEM
Invalid element provided.
mpp_invalid_param#
#define MPP_INVALID_PARAM
Invalid parameter provided.
mpp_err_alloc_mutex#
#define MPP_ERR_ALLOC_MUTEX
Error occured while allocating mutex.
mpp_invalid_mutex#
#define MPP_INVALID_MUTEX
Invalid mutex provided.
mpp_mutex_timeout#
#define MPP_MUTEX_TIMEOUT
Mutex timeout occured.
mpp_mutex_error#
#define MPP_MUTEX_ERROR
Mutex error occured.
mpp_malloc_error#
#define MPP_MALLOC_ERROR
Memory allocation error occured.