Overview
TensorFlow Lite is an open source software library for running machine learning models on mobile and embedded devices. For more information, see www.tensorflow.org/lite.
For memory constrained devices, the library contains TensorFlow Lite for Microcontrollers. For more information, see www.tensorflow.org/lite/microcontrollers.
The MCUXpresso Software Development Kit (MCUXpresso SDK) provides a comprehensive software package with a pre-integrated TensorFlow Lite for Microcontrollers based on version 25-04-08 (from the 8th of April 2025 with commit ). This document describes the steps required to download and start using the library. Additionally, the document describes the steps required to create an application for running pre-trained models.
Note: The document also assumes knowledge of machine learning frameworks for model training.
TensorFlow Lite for Microcontrollers
TensorFlow Lite for Microcontrollers is a port of TensorFlow Lite designed to run machine learning models on DSPs, microcontrollers and other devices with limited memory.
Additional Links:
Build Status
Official Builds
| Build Type | Status | 
|---|---|
| CI (Linux) | |
| Code Sync | 
Community Supported TFLM Examples
This table captures platforms that TFLM has been ported to. Please see New Platform Support for additional documentation.
| Platform | Status | 
|---|---|
| Arduino | |
| Espressif Systems Dev Boards | |
| Renesas Boards | |
| Silicon Labs Dev Kits | |
| Sparkfun Edge | |
| Texas Instruments Dev Boards | 
Community Supported Kernels and Unit Tests
This is a list of targets that have optimized kernel implementations and/or run the TFLM unit tests using software emulation or instruction set simulators.
| Build Type | Status | 
|---|---|
| Cortex-M | |
| Hexagon | |
| RISC-V | |
| Xtensa | |
| Generate Integration Test | 
Contributing
See our contribution documentation.
Getting Help
A Github issue should be the primary method of getting in touch with the TensorFlow Lite Micro (TFLM) team.
The following resources may also be useful:
- SIG Micro email group and monthly meetings. 
- SIG Micro gitter chat room. 
- For questions that are not specific to TFLM, please consult the broader TensorFlow project, e.g.: - Create a topic on the TensorFlow Discourse forum 
- Send an email to the TensorFlow Lite mailing list 
- Create a TensorFlow issue 
- Create a Model Optimization Toolkit issue 
 
Additional Documentation
- Platform/IP support