The NXP lwIP Port
Below is description of possible settings of the port layer and an overview of a few helper functions.
The best place for redefinition of any mentioned macro is lwipopts.h.
The declaration of every mentioned function is in ethernetif.h. Please check
the doxygen comments of those functions before.
Link state
Physical link state (up/down) and its speed and duplex must be read out from PHY over MDIO bus. Especially link information is useful for lwIP stack so it can for example send DHCP discovery immediately when a link becomes up.
To simplify this port layer offers a function ethernetif_probe_link() which
reads those data from PHY and forwards them into lwIP stack.
In almost all examples this function is called every ETH_LINK_POLLING_INTERVAL_MS
(1500ms) by a function probe_link_cyclic().
By setting ETH_LINK_POLLING_INTERVAL_MS to 0 polling will be disabled.
On FreeRTOS, probe_link_cyclic() will be then called on an interrupt generated
by PHY. GPIO port and pin for the interrupt line must be set in the
ethernetifConfig struct passed to ethernetif_init(). On bare metal interrupts
are not supported right now.
Rx task
To improve the reaction time of the app, reception of packets is done in
a dedicated task. The rx task stack size can be set by ETH_RX_TASK_STACK_SIZE
macro, its priority by ETH_RX_TASK_PRIO.
If you want to save memory you can set reception to be done in an interrupt by
setting ETH_DO_RX_IN_SEPARATE_TASK macro to 0.
Disabling Rx interrupt when out of buffers
If ETH_DISABLE_RX_INT_WHEN_OUT_OF_BUFFERS is set to 1, then when the port
gets out of Rx buffers, Rx enet interrupt will be disabled for a particular
controller. Everytime Rx buffer is freed, Rx interrupt will be enabled.
This prevents your app from never getting out of Rx interrupt when the network is flooded with traffic.
ETH_DISABLE_RX_INT_WHEN_OUT_OF_BUFFERS is by default turned on, on FreeRTOS
and off on bare metal.
Limit the number of packets read out from the driver at once on bare metal.
You may define macro ETH_MAX_RX_PKTS_AT_ONCE to limit the number of received
packets read out from the driver at once.
In case of heavy Rx traffic, lowering this number improves the realtime behaviour of an app. Increasing improves Rx throughput.
Setting it to value < 1 or not defining means “no limit”.
Helper functions
If your application needs to wait for the link to become up you can use one of the following functions:
ethernetif_wait_linkup()- Blocks until the link on the passed netif is not up.ethernetif_wait_linkup_array()- Blocks until the link on at least one netif from the passed list of netifs becomes up.
If your app needs to wait for the IPv4 address on a particular netif to become
different than “ANY” address (255.255.255.255) function
ethernetif_wait_ipv4_valid() does this.