Directory structure
The MfgTool for MCU devices is bundled together with the MCU bootloader in <sdk_package>/middleware/mcu-boot
. The following figure provides the mfgtools-rel directory structure on the host PC after the package installation.
MCU bootloader folder hierarchy
In the package, the mfgtools-rel folder appears in the middleware/mcu-boot/bin/tools. blhostis released on MCUBOOT webpage nxp.com/MCUBOOT.
The blhost.exe file appears in the bin/Tools/blhost/win folder and the MfgTool executable MfgTool2.exe appears in the mfgtools-relfolder.
The Profiles folder contains the profile for the MCU bootloader device that includes the OS Firmware folder and the player.inifile.
The files folder in the OS Firmware folder may include the application image along with the custom files to download onto the device.
The ucl2.xml file in the OS Firmware folder is the main XML that the MfgTool processes. It contains the flow of the manufacturing process for the device, which includes the identification parameters for the device and the blhost commands sequenced to query the device and program the image. The example ucl2.xml file is delivered with the USB device identification parameters to identify the MCU bootloader device connected to the PC host and the set of blhost commands required for updating the image on the device. The ucl2.xml file can be customized to suit the custom setup or the manufacturing process flow. The folder contains several example xml files for your reference.
The player.ini file in the ‘Kinetis Bootloader’ profile folder contains configurable parameters for the manufacturing tool application.
The cfg.ini and UICfg.ini files provide the customizable parameters for the look and feel of the tool’s GUI.
The MfgTool.log text file is a useful tool to debug the failures reported in the MfgTool UI. The MfgTool logs the entire command line string it used to invoke the blhost, and also collects the output response text that the blhost puts out on stdout into the MfgTool.log file. The log file is the first place to look into when troubleshooting. The troubleshooting guide section at the end of this document discusses more on the information the tool logs into the MfgTool.log text file.