Connect to the i.MX RT Platform

The i.MX RT platform connects to a host computer to interface with the i.MX RT BootROM application. After the platform connects in serial downloader mode, use the MfgTool to program bootable image into the target flash memory. If both cfg.ini and UlCfg.ini files are configured appropriately, MfgTool recognizes the device and establishes the connection.

The figure below shows that the MfgTool has been connected.

MfgTool GUI with device connected

Parent topic:Program bootable image