Demo applications

The multicore demo applications demonstrate the usage of the MCSDK software components on supported multicore development boards. The following multicore demo applications are located together with other MCUXpresso SDK examples in the <MCUXpressoSDK_install_dir>/boards/<board_name>/multicore_examples… subdirectories.

  • erpc_matrix_multiply_mu

  • erpc_matrix_multiply_mu_rtos

  • erpc_matrix_multiply_rpmsg

  • erpc_matrix_multiply_rpmsg_rtos

  • erpc_two_way_rpc_rpmsg_rtos

  • freertos_message_buffers

  • hello_world

  • multicore_manager

  • rpmsg_lite_pingpong

  • rpmsg_lite_pingpong_rtos

  • rpmsg_lite_pingpong_tzm

The eRPC multicore component can be leveraged for inter-processor communicaton and remote procedure calls between SoCs / development boards. The following multiprocessor demo applications are located together with other MCUXpresso SDK examples in the <MCUXpressoSDK_install_dir>/boards/<board_name>/multiprocessor_examples… subdirectories.

  • erpc_client_matrix_multiply_spi

  • erpc_server_matrix_multiply_spi

  • erpc_client_matrix_multiply_uart

  • erpc_server_matrix_multiply_uart

  • erpc_server_dac_adc

  • erpc_remote_control