IAR
Create an RT1170 M4/RT1180 M7 project
For RT1170, copy the cm4 folder under <install_dir>/boards/evkmimxrt1170/usb_examples/usb_device_hid_mouse/bm/cm4 to the folder where the example must be enabled.
In this case, copy the cm4 folder to <install_dir>/boards/evkmimxrt1170/usb_examples/usb_device_msc_disk/bm.
For RT1180, copy the cm7 folder under <install_dir>/boards/evkmimxrt1180/usb_examples/usb_device_hid_mouse/bm/cm7 to the folder where the example must be enabled.
In this case, copy the cm7 folder to <install_dir>/boards/evkmimxrt1180/usb_examples/usb_device_msc_disk/bm.
For RT1170, open the iar folder under <install_dir>/boards/evkmimxrt1170/usb_examples/usb_device_msc_disk/bm/cm4/iar.
For RT1180, open the iar folder under <install_dir>/boards/evkmimxrt1180/usb_examples/usb_device_msc_disk/bm/cm7/iar.
For RT1170, change the filename
dev_hid_mouse_bm_cm4
todev_msc_disk_bm_cm4
respectively.For RT1180, change the filename
dev_hid_mouse_bm_cm7
todev_msc_disk_bm_cm7
respectively.|
|
4. For RT1170, open the `dev_msc_disk_bm_cm4.eww` and `dev_msc_disk_bm_cm4.ewp` files with a text editor, such as notepad, notepad++, sublime or Visual studio code.
For RT1180, open the `dev_msc_disk_bm_cm7.eww` and `dev_msc_disk_bm_cm7.ewp` files with a text editor, such as notepad, notepad++, sublime or Visual studio code.
5. For RT1170, search and replace all `dev_hid_mouse_bm_cm4` with `dev_msc_disk_bm_cm4`, and then save the files.
|
|
|
|
For RT1180, search and replace all `dev_hid_mouse_bm_cm7` with `dev_msc_disk_bm_cm7`, and then save the files.
|
|
|
|
Rearrange source files
For RT1170, open the cm4 folder under <install_dir>/boards/evkmimxrt1170/usb_examples/usb_device_msc_disk/bm/cm4, and delete all files with the
.c
and.h
extension.For RT1180, open the cm7 folder under <install_dir>/boards/evkmimxrt1180/usb_examples/usb_device_msc_disk/bm/cm7, and delete all files with the
.c
and.h
extension.For RT1170, copy files with the
.c
and.h
extension in the cm7 folder under <install_dir>/boards/evkmimxrt1170/usb_examples/usb_device_msc_disk/bm/cm7 to the cm4 folder under <install_dir>/boards/evkmimxrt1170/usb_examples/usb_device_msc_disk/bm/cm4.|
|
For RT1180, copy files with the `.c` and `.h` extension in the *cm33* folder under *<install\_dir\>/boards/evkmimxrt1180/usb\_examples/usb\_device\_msc\_disk/bm/cm33* to the *cm7* folder under *<install\_dir\>/boards/evkmimxrt1180/usb\_examples/usb\_device\_msc\_disk/bm/cm7*.
|
|
Rearrange project files
Note: The following steps are described for RT1170. However, these steps are also applicable for RT1180.
Open
dev_msc_disk_bm_cm7
anddev_msc_disk_bm_cm4
IAR project respectively. The two workspaces are respectively located under <install_dir>/boards/evkmimxrt1170/usb_examples/usb_device_msc_disk/bm/cm7/iar and <install_dir>/boards/evkmimxrt1170/usb_examples/usb_device_msc_disk/bm/cm4/iar.Compare the whole project directory. Find file groups that are in the
cm7
project but notcm4
and add them to thecm4
project.Compare the two groups with the same name. Delete files that are in the
cm4
project but notcm7
. Find files that are in thecm7
project but notcm4
and add them to thecm4
project. In this case,
For the
board
group, addsdmmc_config
source files toboard
group in thecm4
project.|
|
- For the `component` group, delete files associated with timer from `cm4` project and add no files.
|
|
- For the `drivers` group, delete `fsl_pit` source files from the `cm4` project and add `fsl_usdhc` source files to the `cm4` project.
|
|
- For the `sdmmc` group, there is not `sdmmc` group in the `cm4` project. Add `sdmmc` group and its children to the `cm4` project.
|
|
- For the `source` group, delete the files in the `cm4` source group and add the files under *<install\_dir\>/boards/evkmimxrt1170/usb\_examples/usb\_device\_msc\_disk/bm/cm4* with the same name as in the `cm7` project.
|
|
- For the `usb` group, replace the `hid` group and its children in the `cm4` project with `msc` group in the `cm7` project and delete the `dcd` group.
|
|
Adjust project settings
Note: The following steps are described for RT1170. However, these steps are also applicable for RT1180.
Compare the macro in the project settings: Option - C/C++ compiler > Preprocessor. Add the macro that is in the
cm7
project but notcm4
to thecm4
project.In this case, add the
SD_ENABLED
macro to thecm4
project.|
|
2. Change the include directories in the project settings, by clicking **Option** \> **C/C++ compiler** \> **Preprocessor**, according to the changes of project files.
In this case, delete the directories framed in red and add the directories in green.
|
|
With all above steps done, the RT1170 M7 project successfully changes to an M4 project and the M4 example USB project is available for downloading and debugging. The RT1180 M33 project successfully changes to an M7 project and the M7 example USB project is downloading and debugging.