MCUXpresso SDK Documentation

Vector path enumerations#

This section provides an overview of vector path enumerations.

vg_lite_format_t enumeration#

Values for vg_lite_format_t enum are defined in Table 1.

If vg_lite_format_t

Path data alignment in the array should be:

VG_LITE_S8

8 bit

VG_LITE_S16

2 bytes

VG_LITE_S32

4 bytes

Parent topic:Vector path enumerations

vg_lite_quality_t enumeration#

Specifies the level of hardware assisted anti-aliasing.

Used in structure: vg_lite_path_t.

Used in function: vg_lite_init_path, vg_lite_init_arc_path.

vg_lite_quality_t string values

Description

VG_LITE_HIGH

High quality: 16x coverage sample anti-aliasing

VG_LITE_UPPER

Upper quality: 8x coverage sample anti-aliasing. Use vg_lite_query_feature to determine availability of 8x CSAA (feature enum value gcFEATURE_BIT_VG_QUALITY_8X.(deprecated from June 2020, available with supported hardware from August 2022).

VG_LITE_MEDIUM

Medium quality: 4x coverage sample anti-aliasing

VG_LITE_LOW

Low quality: No anti-aliasing

Parent topic:Vector path enumerations

Parent topic:Vector path control