GATT database
The application must define and populate the database according to its requirements and constraints either statically, at application compile time, or dynamically.
Regardless of how the application creates the GATT database, the following two external references from gatt_database.h must be defined:
/*! The number of attributes in the GATT Database. */
extern uint16_t gGattDbAttributeCount_c;
/*! Reference to the GATT database */
extern gattDbAttribute_t* gattDatabase;
The attribute template is defined as shown here:
**typedef** **struct** {
uint16_t handle ;
/*!< Attribute handle - cannot be 0x0000; attribute handles need not be consecutive, but must be strictly increasing. */
uint16_t permissions ;
/*!< Attribute permissions as defined by ATT. */
uint32_t uuid ;
/*!< The UUID should be read according to the gattDbAttribute_t.uuidType member: for 2-byte and 4-byte UUIDs, this contains the value of the UUID; for 16-byte UUIDs, this is a pointer to the allocated 16-byte array containing the UUID. */
uint8_t * pValue ;
/*!< Pointer to allocated value array. */
uint16_t valueLength ;
/*!< Size of the value array. */
uint16_t uuidType : 2;
/*!< Identifies the length of the UUID; the 2-bit values are interpreted according to the bleUuidType_t enumeration. */
uint16_t maxVariableValueLength : 10;
/*!< Maximum length of the attribute value array; if this is set to 0, then the attribute's length (valueLength) is fixed and cannot be changed. */
} gattDbAttribute_t ;
Parent topic:Prerequisites