Usage

The application is built to work with any other Bluetooth LE device. To showcase the functionality, two platforms are used in the following setup.

  1. Open a serial port terminal and connect them to the two boards, in the same manner described in Testing devices. The start screen is displayed after the board is reset. All LEDs are flashing on both devices.

  2. Configure one of the devices as a GAP peripheral and a Heart Rate server. Change name to HRS. Start advertising on this device.

    BLE Shell>gap devicename HRS
    --> GATTDB Event: Attribute Written
    HRS>gap advdata 1 6
    HRS>gap advdata 8 HRS
    HRS>gap advstart
    HRS>
    --> GAP Event: Advertising parameters successfully set.
    HRS>
    --> GAP Event: Advertising data successfully set.
    HRS>
    --> GAP Event: Advertising state changed successfully!
    HRS>gattdb addservice 0x180D
    --> Heart Rate
    - Heart Rate Measurement Value Handle: 14
    
  3. Configure the other device as a GAP central. Change its name to ‘Collector’. Start scanning and connect to the HRS device by selecting the corresponding device index from the list of scanned devices. In the example below, the HRS device is device number 2. The number of listed scanned devices can be controller through the mShellGapMaxScannedDevicesCount_c define in shell_gap.c.

    nBLE Shell>gap devicename Collector
    --> GATTDB Event: Attribute Written
    Collector>gap scanstart filter
    --> GAP Event: Scan started.
    Collector>
    --> GAP Event: Found device 0 : 880F102F500E 0 dBm
    --> GAP Event: Found device 1 : NXP_CSCS 00049F000006 0 dBm
    --> GAP Event: Found device 2 : HRS 00049F0000FF 0 dBm
    Collector>gap connect 2
    --> GAP Event: Scan stopped.
    Collector>
    --> GAP Event: Connected to peer 0
    
  4. Optionally, the devices can be paired (gAppUsePairing_d and gAppUseBonding_d must be set in app_preinclude.h). On the collector initiate the pairing.

    Collector>gap pair 0
    --> Pairing...
    --> GAP Event: Link Encrypted
    --> GAP Event: Device Paired
    
  5. On the Collector, start service discovery. The device discovers the GAP, GATT, and Heart Rate services.

    Collector>gatt discover 0 -all
    --> Discovered primary services: 3
    --> Generic Attribute Start Handle: 1 End Handle: 4
    - Service Changed Value Handle: 3
    - Client Characteristic Configuration Descriptor Handle: 4
    --> Generic Access Start Handle: 5 End Handle: 11
    - Device Name Value Handle: 7
    - Appearance Value Handle: 9
    - Peripheral Preferred Connection Parameters Value Handle: 11
    --> Heart Rate Start Handle: 12 End Handle: 19
    - Heart Rate Measurement Value Handle: 14
    - Client Characteristic Configuration Descriptor Handle: 15
    - Body Sensor Location Value Handle: 17
    - Heart Rate Control Point Value Handle: 19
    
  6. Configure the HRS to send notifications by writing the CCCD from the Collector. Send a GATT write command with value 1 to the CCCD handle discovered, 15.

    Collector>gatt write 0 15 0x0001
    --> GATT Event: Characteristic Value Written!
    
  7. Send heart rate measurement notifications from the HRS device by using the value handle obtained after adding the service in the previous step.

    HRS>gatt notify 0 14
    
  8. A notification appears on the Collector console.

    Collector>
    --> GATT Event: Received Notification
    Handle: 14
    Value: B400
    

Extended advertising

Use the Bluetooth LE Shell application to exercise the advertising extension features:

On the GAP Peripheral device:

  1. Configure the extended advertising parameters. In the below example, the advertising type is set to connectable and includes TX power and the primary PHY is set to Coded PHY.

  2. Configure the extended advertising data. The Bluetooth LE Shell applications has the feature to send for test, a large data payload. Use the extended advertisement default configuration (not call “gap extadvcfg”), pass the command “gap extadvdata” with no parameters and the default data is added. The length is configurable at compile time through SHELL_EXT_ADV_DATA_SIZE and the data pattern is SHELL_EXT_ADV_DATA_PATTERN. Start the default test with call for “gap extadvstart”.

    The advertising data type is set to shortened local name (8) and the advertising data content is set to test_ext_adv_data.

    Note: Users must note that extended connectable advertising does not allow for chained advertising data. The data length must be limited to what can fit in a single AUX_ADV_IND PDU (251 bytes at maximum). This means that passing the gap extadvdata with no parameters and the default value of SHELL_EXT_ADV_DATA_SIZE (500 bytes) after having set the advertising type to connectable will result in an error when trying to start advertising.

  3. Start extended advertising.

    BLE Shell>gap extadvcfg -type 65 -phy1 3
    BLE Shell>gap extadvdata 8 test_ext_adv_data
    BLE Shell>gap extadvstart
    --> GAP Event: Extended
    Advertising parameters successfully set.
    --> GAP Event:
    Extended Advertising data successfully set.
    --> GAP Event: Advertising state changed successfully!
    
  4. On the GAP Central device

    Set the scanning parameters. The scanning PHY is set to match the advertising PHY, in this case Coded PHY.

  5. Start scanning and filter duplicates.

    BLE Shell>gap scancfg -phy 4
    BLE Shell>gap scanstart filter
    BLE Shell>
    -> GAP Event: Scan started.
    BLE Shell>
    --> GAP Event: Found device 0 : 0060375BCEC6 -23 dBm
    Advertising Extended Data:
    test_ext_adv_data
    
  6. Set the connection initiating PHYs corresponding to the primary PHY on which the advertising is performed.

  7. Connect to the desired device in the scanned devices list.

    BLE Shell>gap connectcfg -phy 4
    --> Connection Parameters:
    --> Connection Interval: 200 ms
    --> Connection Latency: 0
    --> Supervision Timeout: 32000 ms
    --> Connecting PHYs: Coded
    BLE Shell>gap connect 0
    BLE Shell>
    -> GAP Event: Scan stopped.
    BLE Shell>
    --> GAP Event: Connected to peer 0
    

Parent topic:Usage

RSSI Monitor

RSSI Monitor is an application that allows monitoring the RSSI of a remote peer on advertising or connection channel. The GAP peripheral device can modify the output TX power on both advertising and connection channels.

  1. On GAP peripheral device

    Set the primary advertising PHY to Coded PHY. Start advertising and read the address. Set the TX power in dBm to a value less than 20 dBm.

    BLE Shell>gap address
    BLE Shell>
    --> GAP Event: Public Address Read:C4603770BCC5
    BLE Shell>gap extadvcfg -phy1 3
    BLE Shell>gap extadvstart
    BLE Shell>
    --> GAP Event: Extended Advertising parameters successfully set.
    BLE Shell>
    --> GAP Event: Extended Advertising data successfully set.
    BLE Shell>
    --> GAP Event: Advertising state changed successfully!
    BLE Shell>gap txpower adv 0
    BLE Shell>
    --> GAP Event: Success!
    
  2. On GAP Central device

    Set the scanning PHY to Coded PHY. Start monitoring the RSSI on advertising Channel using the address of the Peripheral device. Scanning starts automatically, if it is not previously enabled.

    BLE Shell>gap scancfg -phy 4
    BLE Shell>gap rssimonitor C4603770BCC5--> Reading RSSI on advertising channel:
    BLE Shell>
    -> GAP Event: Scan started.
    BLE Shell>
     RSSI: -27 dBm
     RSSI: -27 dBm
     RSSI: -27 dBm
     RSSI: -27 dBm
     RSSI: -27 dBm
     RSSI: -29 dBm
                            
    

    In the below example, the RSSI in monitored on a connection channel. On GAP Peripheral, start advertising in connectable mode on Coded PHY and adjust the TX power level.

    BLE Shell>gap extadvcfg -type 65 -phy1 3
    BLE Shell>gap extadvdata 8 rssimonitortest
    BLE Shell>gap extadvstart
    BLE Shell>
    --> GAP Event: Extended Advertising parameters successfully set.
    BLE Shell>
    --> GAP Event: Extended Advertising data successfully set.
    BLE Shell>
    --> GAP Event: Advertising state changed successfully!
    BLE Shell>
    --> GAP Event: Connected to peer 0
    BLE Shell>
    --> GAP Event: Advertising stopped!
    BLE Shell>gap txpower conn 10
    BLE Shell>
    --> GAP Event: Success!
    

    On the GAP Central device, start scanning on the Coded PHY. Update the connection PHY also to Coded PHY, then connect to the remote device and monitor continuously the RSSI on the connection channel.

    BLE Shell>gap scancfg -phy 4
    BLE Shell>gap connectcfg -phy 4
    -->  Connection Parameters:
        -->  Connection Interval: 200 ms
        -->  Connection Latency: 0
        -->  Supervision Timeout: 32000 ms
        -->  Connecting PHYs: Coded
    BLE Shell>gap scanstart filter
    BLE Shell>
    ->  GAP Event: Scan started.
    BLE Shell>
    -->  GAP Event: Found device 0 : C4603770BCC5 -21 dBm
     Advertising Extended Data:
    rssimonitortest
    gap connect 0
    BLE Shell>
    ->  GAP Event: Scan stopped.
    BLE Shell>
    -->  GAP Event: Connected to peer 0
    BLE Shell>gap rssimonitor 0 -c
    -->  Reading RSSI from connected device:
    BLE Shell>
     RSSI: -22 dBm
     RSSI: -23 dBm
     RSSI: -21 dBm
     RSSI: -22 dBm
     RSSI: -22 dBm
    BLE Shell>gap rssistop
    
  3. Update the PHY preference and continue monitoring the RSSI. For coded PHY, the coding scheme can be configured between S2 and S8 (500 kbit/s and 125 kbit/s).

    BLE Shell>gap phy 0 -tx 4 -rx 4 -o 1
    BLE Shell>
    --> GAP Event: Phy update complete with peer 0
    --> TxPhy: Coded
    --> RxPhy: Coded
    
    BLE Shell>gap phy 0 -tx 2 -rx 2
    BLE Shell>
    --> GAP Event: Phy update complete with peer 0
    --> TxPhy: 2M
    --> RxPhy: 2M
    
    BLE Shell>gap rssimonitor 0 -c
    --> Reading RSSI from connected device:
    BLE Shell>
    RSSI: -23 dBm
    RSSI: -23 dBm
    RSSI: -21 dBm
    RSSI: -21 dBm
    --> GAP Event: Phy update complete with peer 0
    --> TxPhy: Coded
    --> RxPhy: Coded
    
    BLE Shell>
    RSSI: -22 dBm
    RSSI: -21 dBm
    RSSI: -22 dBm
    RSSI: -23 dBm
    RSSI: -23 dBm
    --> GAP Event: Phy update complete with peer 0
    --> TxPhy: 2M
    --> RxPhy: 2M
    BLE Shell>
    RSSI: -22 dBm
    RSSI: -21 dBm
    RSSI: -21 dBm
    RSSI: -20 dBm
    

Parent topic:Usage

Parent topic:Bluetooth LE Shell