BDB_tsFindAndBindEvent#
The following structure contains the data for a ‘Finding and Binding’ event (see Section 2.9), which is passed to the application during the Finding and Binding process on the initiator.
typedef struct{
uint8 u8InitiatorEp;
uint8 u8TargetEp;
uint16 u16TargetAddress;
uint16 u16ProfileId;
uint16 u16DeviceId;
uint8 u8DeviceVersion;
union {
uint16 u16ClusterId;
uint16 u16GroupId;
}uEvent;
ZPS_tsAfZdpEvent *psAfZdpEvent;
bool bAllowBindOrGroup;
bool bGroupCast;
}BDB_tsFindAndBindEvent;
where:
u8InitiatorEpis the number of the endpoint involved in the binding/grouping on the initiator node.u8TargetEpis the number of the endpoint involved in the binding/grouping on the target node.u16TargetAddressis the 16-bit network address of the target node.u16ProfileIdis the identifier of the ZigBee application profile supported by the two nodes (for Lighting & Occupancy devices, this is 0x0104)u16DeviceIdis the 16-bit identifier of the ZigBee device type supported by the target endpoints. This must be a device type identifier issued by the ZigBee Alliance.u8DeviceVersioncontains 4 bits (bits 0-3) representing the version of the supported device description on the target node (the default is 0000, unless set to another value according to the application profile used).uEventis a union of the following two fields:u16ClusterIdis the identifier of the cluster involved in the binding.u16GroupIdis the address of the group to which the target endpoint is assigned.
psAfZdpEventis a pointer to a ZPS_tsAfZdpEvent structure containing the generated Finding and Binding event - this ZPS structure is detailed in the ZigBee 3.0 Stack User Guide (JNUG3130). The event can be any of the following (detailed in Section 2.9):BDB_EVENT_FB_HANDLE_SIMPLE_DESC_RESP_OF_TARGET
BDB_EVENT_FB_CHECK_BEFORE_BINDING_CLUSTER_FOR_TARGET
BDB_EVENT_FB_CLUSTER_BIND_CREATED_FOR_TARGET
BDB_EVENT_FB_BIND_CREATED_FOR_TARGET
BDB_EVENT_FB_GROUP_ADDED_TO_TARGET
BDB_EVENT_FB_ERR_BINDING_FAILED
BDB_EVENT_FB_ERR_BINDING_TABLE_FULL
BDB_EVENT_FB_ERR_GROUPING_FAILED
BDB_EVENT_FB_NO_QUERY_RESPONSE
BDB_EVENT_FB_TIMEOUT
bAllowBindOrGroupis a Boolean flag that indicates whether the relevant cluster is permitted to participate in a binding or grouping. The default value is TRUE (permitted) but if the application must exclude the cluster (and block the binding/grouping) then it should set this field to FALSE.bGroupCastis a Boolean flag that indicates whether an ‘Add Group If Identifying’ command should be broadcast to all the identifying targets (TRUE) or an ‘Add Group’ request should be individually unicast to all the identifying targets. The default value is TRUE.
Parent topic:Structures