BDB_tsOobWriteDataToAuthenticate#
The following structure contains authentication data that is used to encrypt a security key during out-of-band commissioning of the node.
typedef struct{
uint64 u64ExtAddr;
uint8* pu8InstallCode;
}BDB_tsOobWriteDataToAuthenticate;
where:
u64ExtAddris the IEEE/MAC address of the node.pu8InstallCodeis a pointer to a 16-bit install code to be used in the key encryption.
Parent topic:Structures