MCUXpresso SDK Documentation

Network security#

The ZigBee Base Device supports the following network security modes:

  • Centralized security

  • Distributed security

These security modes are described in the subsections below:

All Router and End Device nodes should support both centralized security and distributed security by adapting to the security scheme employed by the network that they join. A Co-ordinator supports only centralized security.

When the application calls BDB_vInit(), this function internally calls the function BDB_vSetKeys(). This function loads the appropriate pre-configured link key, depending on whether the node type supports centralized and/or distributed security. The pre-configured link keys are defined in the file bdb_link_keys.c.

Centralized security networks#

A centralized security network is formed by a Coordinator, which also acts as the Trust Centre for the network. When a node attempts to join the network, it is authenticated by this Trust Centre before it is allowed into the network.

For participation in centralized security networks, all nodes must be pre-configured with a link key. This key is used to encrypt the network key when passing it from the Trust Centre to a newly joined node. When a node joins a network with centralized security, the ZigBee Base Device automatically uses the relevant pre-configured link key. Similar is the case for a Coordinator that forms a new centralized security network.

The following key types can be pre-configured for centralized security:

  • Default Global Trust Centre Link Key: This key is factory-programmed into all nodes and is used to encrypt communications between the Trust Centre and a joining node.

  • Touchlink Pre-configured Link Key: This key is factory-programmed into all nodes that can employ Touchlink commissioning and is used to encrypt communications between the Router parent and a joining node. The Touchlink Pre-configured Link Key can be one of three types:

    • Development key, used during development before ZigBee certification

    • Master key, used after successful ZigBee certification

    • Certification key, used during ZigBee certification testing

      • The link key used in the final products should be a ‘master key’, which results from the successful ZigBee certification of the product.

  • Install Code-derived Pre-configured Link Key: This key is derived by the ZigBee stack from a random install code which is assigned to each Router and End Device node in the factory. The install code is factory-programmed into the node but provided to the Trust Centre via out-of-band means when the node is commissioned. The use of install codes is described in more detail below.

Install Codes#

An install code is used to create an initial link key employed in commissioning an individual node into a centralized security network. An install code is assigned to the node in the factory. It is a random code but is not necessarily unique (the same install code may be randomly generated for more than one node). The ZigBee stack derives a link key from the install code using a Matyas-Meyer-Oseas hash function. The install code is factory-programmed into the node and also accompanies the node (for example: in printed form) when it leaves the factory. The process of using an install code to commission a node is outlined below.

In the factory:

  1. An install code is randomly generated for the individual node.

  2. The install code is programmed into the node.

  3. A pre-configured link key is derived from the install code by the ZigBee stack.

  4. The install code is shipped with the node (by some unspecified means).

During installation:

  1. The install code that was shipped with the node is installed into the Co-ordinator/Trust Centre.

  2. The pre-configured link key is derived from the install code by the ZigBee stack of the Co-ordinator/Trust Centre.

  3. The Trust Centre and node then use the pre-configured link key in joining the node to the network (for example: to encrypt/decrypt the network key).

More detailed information about install codes are available in the ZigBee Base Device Behavior Specification (13-0402-08).

Parent topic:Network security

Distributed security networks#

A distributed security network is formed by a Router and does not have a Trust Centre. It consists only of Routers and End Devices. When a node attempts to join the network, it is authenticated by its Router parent before it is allowed into the network.

For participation in distributed security networks, all Router and End Device nodes must be pre-configured with a link key. This key is used to encrypt the network key when passing it from a Router parent to a newly joined node. When a Router or End Device joins a network with distributed security, the ZigBee Base Device automatically uses the relevant pre-configured link key. Similar is the case for a Router that forms a new distributed security network.

The following key types can be pre-configured for distributed security:

  • Distributed Security Global Link Key: This key is factory-programmed into all nodes and is used to encrypt communications between the Router parent and a joining node.

  • Touchlink Pre-configured Link Key: This key is factory-programmed into all nodes that can employ Touchlink commissioning and is used to encrypt communications between the Router parent and a joining node. The Touchlink Pre-configured Link Key can be one of three types:

    • Development key, used during development before ZigBee certification

    • Master key, used after successful ZigBee certification

    • Certification key, used during ZigBee certification testing

      • The link key used in the final products should be a ‘master key’, which results from the successful ZigBee certification of the product.

Parent topic:Network security

Parent topic:ZigBee Base Device