Overview

The NXP Serial Memory Tool is a Visual Studio Code extension that streamlines serial memory configuration and validation for NXP microcontrollers. With an intuitive graphical interface, developers can easily configure memory parameters, validate settings on real hardware, and generate FCB binaries—all without leaving VS Code.

Note: This user guide is for NXP Serial Memory Tool version 26.07. For the latest updates and information, check the extension marketplace page.

Note: The software is subject to the NXP software license agreement.

Key features

  • Serial memory configuration and validation

  • Real-time validation

  • Integration with Visual Studio Code

  • Import/save capability

  • Flash Configuration Block (FCB) generation (for supported devices)

  • User-friendly user interface (UI) for creating and modifying the memory lookup table

  • Link a C project to apply configuration changes (for supported devices)

  • Provides automatic memory‑chip parameter discovery via the Serial Flash Discoverable Parameters (SFDP) Test (for supported devices)

  • Simplified configuration mode using configuration words, providing an alternative to the Advanced configuration mode (for supported devices)

  • Collapse/Expand all configuration sections for streamlined navigation

  • Filter settings search box to quickly locate specific configuration parameters

  • Scroll to top button for easy navigation in long configuration views

  • Settings modification counter with reset to default option, with visual highlighting of modified fields

  • Validation marker in the top-right side to show the current configuration status: Valid or Invalid

  • GitHub Copilot Integration (requires VS Code 1.99+) — Configure device, memory, and mode directly from the Copilot Chat panel using natural language, guided wizards, or artificial intelligence (AI)-driven agent mode (Experimental)

System requirements

Supported operating systems

  • Windows 11 (64-bit)

Software requirements

  • Visual Studio Code (the latest version is recommended)

  • Python environment (the tool configures this automatically)

Hardware support

  • i.MX RT101x series

  • i.MX RT102x series

  • i.MX RT1024 series

  • i.MX RT105x series

  • i.MX RT106x series

  • i.MX RT118x series

  • i.MX RT7xxx series

  • RW61x series

Installation

Installing the extension

  • Open Visual Studio Code

  • Go to the Extensions view (Ctrl+Shift+X)

  • Search for “Serial Memory Tool for VS Code”

  • Click Install

Setting up the Python environment

  1. After installation, the Install Toolchain button appears in the tool interface.

Install toolchain

  1. To automatically set up the preconfigured Python environment, click the button.

  2. Wait for the installation to complete (this process may take several minutes).

Install toolchain notification

  1. Once the installation is complete, the tool interface is fully loaded and ready to use. The Welcome page displays the Manage Toolchains option, which allows you to manage your toolchain installation.

Manage toolchains

Getting started

Working with Serial Memory Tool

1. Open VS Code

  • Launch Visual Studio Code on your system

2. Access the Serial Memory Tool

  • Look for the NXP tool icon in the Activity Bar

Toolbar

  • Or open the Command Palette (Ctrl+Shift+P) and search for “Serial Memory Tool”

3. Select the target device

  • Select a processor from the supported devices list.

  • Once a processor is selected, a default Memory Chip is automatically assigned. This chip comes with a standard configuration validated on the EVK board.

  • For supported devices, a toggle button enables switching between Simplified and Advanced configuration modes.

MCU and memory

  • If the Memory Chip is changed, the memory type is updated automatically in the Configuration page to match the new selection.

Memory chip type

4. Use the default configuration or create a custom configuration

  • EVK configuration is set by default for the selected device.

  • Core configuration allows you to modify core-specific parameters as frequency, caches and prefetch.

Core configuration

4.1. Advanced configuration mode

  • This mode provides full control over memory parameters.

  • If needed, adjust the configuration of Memory, FlexSPI Connection, Memory LUT.

  • Memory Information Configuration

Memory information configuration

  • FlexSPI Connection Configuration

Flexspi connection configuration

  • Memory LUT Configuration provides the option to add or remove LUT commands as needed for advanced memory configurations.

Memory lut configuration

4.2. Simplified configuration mode

  • This mode is intended for standard configurations and reduces complexity compared to Advanced mode.

  • Select configuration words from the drop-down menu to quickly apply predefined memory settings.

Simplified configuration mode

4.3. Configuration navigation and management tools

  • Collapse/Expand All — Use the collapse/expand toggle to show or hide all configuration sections at once. This is useful when working with large configurations and you want to focus on specific sections.

Collapse/Expand All

  • Filter Settings — Use the search box at the top of the Configuration panel to filter settings by name. As you type, only matching parameters are displayed, making it easy to locate a specific setting without scrolling through all sections.

Filter Settings

  • Scroll to Top — When scrolling down through the configuration, a Scroll to Top button appears, allowing you to quickly return to the top of the Configuration panel. Clicking it scrolls the view back to the top of the panel instantly.

Scroll to Top

  • Modification Counter and Reset to Default — A counter displays the number of settings that have been modified from their default values. Modified fields are visually highlighted in the configuration panel, making it easy to identify which parameters have been changed. Click the Reset to Default button to restore all configuration parameters to their original default values for the selected device and memory chip.

Modification Counter and Reset to Default

  • Validation Status — A validation badge appears in the top-right corner of the Configuration panel, indicating the current configuration status. The badge shows Valid when all parameters are correctly configured, or Error(s) when one or more settings contain invalid values. This provides immediate visual feedback on whether the configuration can be used for testing or FCB generation without running a full validation.

Validation Status

4.4. To save any configuration changes, press Ctrl+S or navigate to File->Save.

Save configuration

5. Working with GitHub Copilot (Experimental)

  • The Serial Memory Tool integrates with GitHub Copilot Chat, allowing you to configure your device setup directly from the chat panel using @smt.

Interaction Modes

Mode

Command

Description

Guided Wizard

@smt /setup

Step-by-step configuration with clickable follow-up buttons

Quick Setup

@smt /setup quick

Fast configuration using VS Code dropdown menus

Natural Language

@smt set device RT118X

Set device, mode, or memory using plain English

Status

@smt /status

Show current configuration summary

Agent Mode

Free text in Agent mode

Copilot autonomously calls the right tools

Guided wizard — type @smt /setup and follow the clickable buttons:

Setup Wizard

Natural language — configure everything in one sentence:

SMT Natural Language

7. Board detection

  • Before connecting, ensure the board is configured to boot in Serial Downloader mode.

  • Connect one cable to the USB_OTG1 for the Serial Downloader interface and the second cable to the Debug USB port for UART communication.

  • Detect a connected board using the “Refresh current connection” button in the Connection group.

Refresh connection

  • Choose the appropriate COM port in case multiple boards are connected.

  • The connection icon changes and indicates the Connected status once the tool detects the board.

Board detection

8. Validate configuration by executing tests on the target

Configure test parameters:

  • Click Test, the Test Configuration tab opens to the right.

  • To modify test settings, change test parameters.

  • When test parameters change, validation errors appear if the selected parameters are incorrect.

Test configuration

Execute test:

  • Tests cannot run unless the tool detects a board (the Run Test button is disabled).

  • Once the tool detects a board, the Run button becomes enabled (green icon).

  • Click the Start button to start the test execution.

  • The pass/fail status icon appears on the left side of the tests tree after the test finishes executing.

Test execution

  • The test result also appears in the Test Result panel.

Test result

  • For the SFDP test, the tool generates a detailed report showing memory parameters detected from the device.

SFDP table

9. Test logging

  • The test execution log appears in the Serial Memory Tool for VS Code console, which opens automatically at the bottom when a test starts.

  • Upon test completion, the tool generates a summary report displaying the overall test results. A notification appears with options to open the log file or log folder.

Test logging

10. Import configuration

  • The Import button is located in the top-right corner in the “MCU & Memory” panel.

  • Imported -> A saved configuration can be imported using the import button.

Import configuration

11. Generate FCB

  • The FCB button is available in the top-right corner in the “MCU & Memory” panel.

  • To generate and save FCB binary, use the Generate FCB button.

Generate FCB

Basic workflow

Start Tool → Select MCU and Memory Chip → Configure Memory Settings → Board detection → Validate Configuration by executing tests on target -> Generate FCB or save configuration

Basic Workflow

User interface overview

Main interface components

Welcome panel

The Welcome Panel is located in the top-right corner of the interface and serves as the starting point for toolchain management and initial setup. It provides access to options such as installing and managing the toolchain, allowing users to configure their development environment. Through this panel, it is possible execute commands to install the toolchain, uninstall it if needed, and check for available updates to ensure the setup remains current and functional.

Device selection panel (MCU & Memory)

This panel is located at the top of the interface, making it easily accessible as the starting point for configuration. The panel allows choosing the target microcontroller unit (MCU) and the memory chip you intend to work with. This selection is essential for tailoring the configuration and generation process to your specific hardware setup. Currently, the RT1180 microcontroller is available for selection. Additional devices will be supported in future updates.

Panel sections:

  • MCU Device selection: Choose the microcontroller that matches your project requirements.

  • Memory Chip selection: Select the memory chip that will be paired with the chosen MCU.

  • Import / Save / Generate FCB Buttons: Use these buttons to import existing configurations, save your current setup, or generate the Flash Configuration Block (FCB) based on your selections.

Configuration panel

The Configuration Panel is located in the center area of the interface and is used to set up parameters for serial memory.

Panel sections:

  • Core Configuration

  • Memory Information Configuration

  • FlexSPI connection configuration

  • Memory LUT Configuration

Panel tools:

  • Collapse/Expand All: A toggle control that collapses or expands all configuration sections simultaneously. When collapsed, only section headers are visible, providing a compact overview. When expanded, all parameters within each section are displayed for detailed editing.

Collapse/Expand All

  • Filter settings: A search box located at the top of the Configuration panel. Typing a keyword filters the visible settings in real time, showing only parameters whose names match the search query. Clear the search box to restore the full view.

Filter Settings

  • Scroll to Top: A floating button that appears automatically when the user scrolls down within the Configuration panel. Clicking it scrolls the view back to the top of the panel instantly.

Scroll to Top

  • Modification Counter and Reset to Default: A badge or indicator that shows how many configuration parameters have been changed from their default values. Modified fields are highlighted in the configuration panel, making it easy to identify changed parameters. Next to it, a Reset to Default button restores all settings to the factory defaults for the currently selected device and memory chip combination. This is useful when experimenting with configurations and you need to return to a known good state.

Modification Counter and Reset to Default

  • Validation Status: A badge in the top-right corner of the Configuration panel that indicates the current configuration validity. It shows Valid when all parameters are correctly configured, or Error(s) when one or more settings contain invalid values. This gives immediate visual feedback on the configuration status without running a full test.

Validation Status

Tests panel

The Tests panel is located on the right side of the center area and displays validation results and errors. It provides feedback on the correctness of the configuration and indicates whether the current setup passes or fails. This helps users identify and resolve issues, ensuring an accurate configuration process.

Connection panel

The Connection panel appears at the bottom right of the interface and detects whether a development board is connected. It shows the current connection status and allows users to manually refresh the connection by clicking the Refresh connection button. This helps ensure that the system is properly linked to the hardware before proceeding with further configuration or testing.

Troubleshooting

This chapter contains known problems and recommended solutions.

Issue: tool does not start

Symptoms: Extension loads but the tool interface does not appear.

Solutions:

  1. Restart VS Code

  2. Check if Python environment is properly installed

  3. Run “Manage Toolchain” and Reset Toolchain

  4. Reinstall Toolchain using “Install Toolchain” button

  5. Check VS Code output panel for error messages

Issue: device is not recognized

Symptoms: RT1180 does not appear in the device list.

Solutions:

  1. Make sure to use a supported Windows version

  2. Update the extension to the latest version

  3. Check system requirements

Known issues and limitations

This chapter contains limitations and possible workarounds.

Current limitations

  1. Operating system support:

  • Currently supported only on Windows 10/11 (64-bit)

  • macOS and Linux support is planned for future releases

  1. Device support:

  • Limited to the microcontroller families listed in the Hardware support section

  • Additional device support is in development

  1. Feature limitations:

  • FCB generation is available only for supported devices

  • SFDP test table generation is available only for supported devices

  • Linking a C project is available only for supported devices

  • Simplified mode is available only for supported devices

Workarounds

Unsupported operating systems

  • Use a Windows virtual machine

  • Wait for future OS support updates

Additional device support

  • Check for extension updates regularly

  • Contact NXP support for roadmap information

References

  1. Documentation:

  1. Online resources:

  1. Technical support:

Revision history

Document ID

Release date

Description

UG10328 v.7.0

31 July 2026

Updated for 26.07.

UG10328 v.6.0

30 June 2026

Updated for 26.06.

UG10328 v.5.0

31 May 2026

Updated for 26.05.

UG10328 v.4.0

30 April 2026

Updated for 26.04.

UG10328 v.3.0

31 March 2026

Updated for 26.03.

UG10328 v.2.0

12 December 2025

Updated for 25.12.

UG10328 v.1.0

4 December 2025

Initial version.

Note about the source code in the document

Example code shown in this document has the following copyright and BSD-3-Clause license:

Copyright 2026 NXP Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

  1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

  2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

  3. Neither the name of the copyright holder nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS “AS IS” AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.