![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The Driver_GPIO.h file contains the definitions for GPIO Driver direction. More...
#include "Driver_Common.h"

Go to the source code of this file.
Data Structures | |
| struct | GENERIC_DRIVER_GPIO |
| Access structure of the GPIO Driver. More... | |
Macros | |
| #define | GPIO_API_VERSION ARM_DRIVER_VERSION_MAJOR_MINOR(2, 0) /* API version */ |
Typedefs | |
| typedef enum gpio_direction_en | gpio_direction_t |
| typedef void * | pinID_t |
| GPIO Driver direction. More... | |
| typedef ARM_DRIVER_VERSION | GENERIC_DRIVER_VERSION |
| typedef void(* | gpio_isr_handler_t) (void *apUserData) |
| typedef struct GENERIC_DRIVER_GPIO | GENERIC_DRIVER_GPIO |
| Access structure of the GPIO Driver. More... | |
Enumerations | |
| enum | gpio_direction_en { GPIO_DIRECTION_IN = 0U, GPIO_DIRECTION_OUT = 1U } |
The Driver_GPIO.h file contains the definitions for GPIO Driver direction.
Definition in file Driver_GPIO.h.
| #define GPIO_API_VERSION ARM_DRIVER_VERSION_MAJOR_MINOR(2, 0) /* API version */ |
Definition at line 40 of file Driver_GPIO.h.
| typedef struct GENERIC_DRIVER_GPIO GENERIC_DRIVER_GPIO |
Access structure of the GPIO Driver.
| typedef ARM_DRIVER_VERSION GENERIC_DRIVER_VERSION |
Definition at line 58 of file Driver_GPIO.h.
| typedef enum gpio_direction_en gpio_direction_t |
| typedef void(* gpio_isr_handler_t) (void *apUserData) |
Definition at line 60 of file Driver_GPIO.h.
| typedef void* pinID_t |
GPIO Driver direction.
Definition at line 56 of file Driver_GPIO.h.
| enum gpio_direction_en |
| Enumerator | |
|---|---|
| GPIO_DIRECTION_IN | IN. |
| GPIO_DIRECTION_OUT | OUT. |
Definition at line 47 of file Driver_GPIO.h.