![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
Provides init() and read() functions for the FXLS8952 3-axis accelerometer. More...
#include "board.h"#include "sensor_fusion.h"#include "sensor_io_i2c.h"#include "sensor_drv.h"#include "FXLS8952.h"#include "drivers.h"
Go to the source code of this file.
Macros | |
| #define | FXLS8952_COUNTSPERG 512 |
| #define | FXLS8952_ACCEL_FIFO_SIZE 32 |
Provides init() and read() functions for the FXLS8952 3-axis accelerometer.
Definition in file driver_FXLS8952.c.
| #define FXLS8952_ACCEL_FIFO_SIZE 32 |
Definition at line 46 of file driver_FXLS8952.c.
| #define FXLS8952_COUNTSPERG 512 |
Definition at line 45 of file driver_FXLS8952.c.