![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
Provides init() and read() functions for the MPL3115 pressure sensor/altimeter. More...
#include "board.h"#include "sensor_fusion.h"#include "sensor_io_i2c.h"#include "mpl3115_drv.h"#include "drivers.h"
Go to the source code of this file.
Macros | |
| #define | MPL3115_MPERCOUNT 0.0000152587890625F |
| #define | MPL3115_CPERCOUNT 0.00390625F |
| #define | MPL3115_ACCEL_FIFO_SIZE 32 |
Provides init() and read() functions for the MPL3115 pressure sensor/altimeter.
Definition in file driver_MPL3115.c.
| #define MPL3115_ACCEL_FIFO_SIZE 32 |
Definition at line 46 of file driver_MPL3115.c.
| #define MPL3115_CPERCOUNT 0.00390625F |
Definition at line 45 of file driver_MPL3115.c.
| #define MPL3115_MPERCOUNT 0.0000152587890625F |
Definition at line 44 of file driver_MPL3115.c.