![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
Provides a simple abstraction for a periodic interval timer. More...

Go to the source code of this file.
Functions | |
| void | pit_init (uint32_t microseconds) |
Variables | |
| volatile bool | pitIsrFlag |
Provides a simple abstraction for a periodic interval timer.
Bare metal implementations of the sensor fusion library require at least one periodic interrupt for use as a timebase for sensor fusion functions. The Periodic Interval Timer (PIT) is one such module that is commonly found on NXP Kinetis MCUs. The PIT functions are only referenced at the main() level. There is no interaction within the fusion routines themselves.
Definition in file driver_pit.h.
| void pit_init | ( | uint32_t | microseconds | ) |
Definition at line 70 of file driver_pit.c.
References PIT_IRQ_ID, and PIT_SOURCE_CLOCK.
Referenced by main().

| volatile bool pitIsrFlag |
Definition at line 61 of file driver_pit.c.
Referenced by main(), and PIT_LED_HANDLER().