43 #ifndef __ISSDK_HAL_H__ 44 #define __ISSDK_HAL_H__ 46 #include "fsl_lpsci_cmsis.h" 47 #include "fsl_i2c_cmsis.h" 48 #include "fsl_spi_cmsis.h" 53 #endif // __ISSDK_HAL_H__ The frdm_kl25z.h file defines GPIO pin mappings for FRDM-KL25Z board.
The frdm_stbc_a8471_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-kl25...