![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The frdm_stbc_a8471_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-kl25z and frmd-stbc-a8471 shield. More...

Go to the source code of this file.
Macros | |
| #define | SHIELD_NAME "FRDMSTBC-A8471" |
| #define | FXLS8471_INT1 D2 |
| #define | FXLS8471_INT2 D8 |
| #define | FXLS8471_SPI_CS D10 |
The frdm_stbc_a8471_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-kl25z and frmd-stbc-a8471 shield.
Definition in file frdm_stbc_a8471_shield.h.
| #define FXLS8471_INT1 D2 |
Definition at line 48 of file frdm_stbc_a8471_shield.h.
| #define FXLS8471_INT2 D8 |
Definition at line 49 of file frdm_stbc_a8471_shield.h.
| #define FXLS8471_SPI_CS D10 |
Definition at line 50 of file frdm_stbc_a8471_shield.h.
| #define SHIELD_NAME "FRDMSTBC-A8471" |
Definition at line 45 of file frdm_stbc_a8471_shield.h.