![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|

Go to the source code of this file.
Macros | |
| #define | SHIELD_NAME "FRDMSTBC-A8491" |
| #define | MMA8491_I2C_ADDR 0x55 |
| #define | MMA8491_EN A1 |
| #define | MMA8491_XOUT D2 |
| #define | MMA8491_YOUT D5 |
| #define | MMA8491_ZOUT D8 |
| #define MMA8491_EN A1 |
Definition at line 48 of file frdm_stbc_a8491_shield.h.
| #define MMA8491_I2C_ADDR 0x55 |
Definition at line 47 of file frdm_stbc_a8491_shield.h.
| #define MMA8491_XOUT D2 |
Definition at line 49 of file frdm_stbc_a8491_shield.h.
Referenced by main().
| #define MMA8491_YOUT D5 |
Definition at line 50 of file frdm_stbc_a8491_shield.h.
Referenced by main().
| #define MMA8491_ZOUT D8 |
Definition at line 51 of file frdm_stbc_a8491_shield.h.
Referenced by main().
| #define SHIELD_NAME "FRDMSTBC-A8491" |
Definition at line 44 of file frdm_stbc_a8491_shield.h.