![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The frdm_stbc_p3115_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-kl25z and frmd-stbc-p3115 shield. More...

Go to the source code of this file.
Macros | |
| #define | SHIELD_NAME "FRDMSTBC-P3115" |
| #define | MPL3115_I2C_ADDR 0x60 |
| #define | MPL3115_INT1 D5 |
| #define | MPL3115_INT2 D2 |
The frdm_stbc_p3115_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-kl25z and frmd-stbc-p3115 shield.
Definition in file frdm_stbc_p3115_shield.h.
| #define MPL3115_I2C_ADDR 0x60 |
Definition at line 48 of file frdm_stbc_p3115_shield.h.
| #define MPL3115_INT1 D5 |
Definition at line 49 of file frdm_stbc_p3115_shield.h.
| #define MPL3115_INT2 D2 |
Definition at line 50 of file frdm_stbc_p3115_shield.h.
| #define SHIELD_NAME "FRDMSTBC-P3115" |
Definition at line 45 of file frdm_stbc_p3115_shield.h.