![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|

Go to the source code of this file.
Macros | |
| #define | SHIELD_NAME "FRDM-STBC-SA9500" |
| The frdm_stbc_sa9500_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-k22f and frmd-stbc-agm01 shield. More... | |
| #define | FXLC95000_I2C_ADDR 0x4C |
| #define | FXLC95000_INT1 D2 |
| #define | FXLC95000_PDB_B D8 |
| #define | FXLC95000_SSB_IO3 D10 |
| #define | FXLC95000_RST_GPIO A3 |
| #define FXLC95000_I2C_ADDR 0x4C |
Definition at line 47 of file frdm_stbc_sa9500_shield.h.
| #define FXLC95000_INT1 D2 |
Definition at line 48 of file frdm_stbc_sa9500_shield.h.
| #define FXLC95000_PDB_B D8 |
Definition at line 49 of file frdm_stbc_sa9500_shield.h.
Referenced by main().
| #define FXLC95000_RST_GPIO A3 |
Definition at line 51 of file frdm_stbc_sa9500_shield.h.
Referenced by main().
| #define FXLC95000_SSB_IO3 D10 |
Definition at line 50 of file frdm_stbc_sa9500_shield.h.
Referenced by main().
| #define SHIELD_NAME "FRDM-STBC-SA9500" |
The frdm_stbc_sa9500_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-k22f and frmd-stbc-agm01 shield.
File: frdm_stbc_sa9500_shield.h
Definition at line 44 of file frdm_stbc_sa9500_shield.h.