![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The gpio_driver_irq_ke15z.c file containes the Generic IRQ implmentation for the FRDM-KE15Z GPIO. More...

Go to the source code of this file.
Functions | |
| void | ksdk_gpio_handle_interrupt (GPIO_Type *base, port_number_t portNumber) |
| void | PORTAE_IRQHandler (void) |
| void | PORTBCD_IRQHandler (void) |
The gpio_driver_irq_ke15z.c file containes the Generic IRQ implmentation for the FRDM-KE15Z GPIO.
Definition in file gpio_driver_irq_ke15z.c.
| void ksdk_gpio_handle_interrupt | ( | GPIO_Type * | base, |
| port_number_t | portNumber | ||
| ) |
Definition at line 179 of file gpio_driver.c.
Referenced by PORTAE_IRQHandler(), and PORTBCD_IRQHandler().

| void PORTAE_IRQHandler | ( | void | ) |
Definition at line 48 of file gpio_driver_irq_ke15z.c.
References GPIO_PORT_NUM, GPIO_TYPE, and ksdk_gpio_handle_interrupt().

| void PORTBCD_IRQHandler | ( | void | ) |
Definition at line 53 of file gpio_driver_irq_ke15z.c.
References GPIO_PORT_NUM, GPIO_TYPE, and ksdk_gpio_handle_interrupt().