![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The PressureSensor structure stores raw and processed measurements for an altimeter. More...
#include <sensor_fusion.h>

Data Fields | |
| uint8_t | iWhoAmI |
| sensor whoami More... | |
| bool | isEnabled |
| true if the device is sampling More... | |
| int32_t | iH |
| most recent unaveraged height (counts) More... | |
| int32_t | iP |
| most recent unaveraged pressure (counts) More... | |
| float | fH |
| most recent unaveraged height (m) More... | |
| float | fT |
| most recent unaveraged temperature (C) More... | |
| float | fmPerCount |
| meters per count More... | |
| float | fCPerCount |
| degrees Celsius per count More... | |
| int16_t | iT |
| most recent unaveraged temperature (counts) More... | |
The PressureSensor structure stores raw and processed measurements for an altimeter.
The PressureSensor structure stores raw and processed measurements, as well as metadata for a pressure sensor/altimeter.
Definition at line 200 of file sensor_fusion.h.
| float fCPerCount |
degrees Celsius per count
Definition at line 209 of file sensor_fusion.h.
| float fH |
most recent unaveraged height (m)
Definition at line 206 of file sensor_fusion.h.
Referenced by fInit_1DOF_P_BASIC(), and fRun_1DOF_P_BASIC().
| float fmPerCount |
meters per count
Definition at line 208 of file sensor_fusion.h.
| float fT |
most recent unaveraged temperature (C)
Definition at line 207 of file sensor_fusion.h.
Referenced by fInit_1DOF_P_BASIC(), and fRun_1DOF_P_BASIC().
| int32_t iH |
most recent unaveraged height (counts)
Definition at line 204 of file sensor_fusion.h.
| int32_t iP |
most recent unaveraged pressure (counts)
Definition at line 205 of file sensor_fusion.h.
| bool isEnabled |
true if the device is sampling
Definition at line 203 of file sensor_fusion.h.
| int16_t iT |
most recent unaveraged temperature (counts)
Definition at line 210 of file sensor_fusion.h.
| uint8_t iWhoAmI |
sensor whoami
Definition at line 202 of file sensor_fusion.h.