![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
This structure defines the mpl3115 data buffer in Altitude Mode. More...
#include <mpl3115_drv.h>

Data Fields | |
| uint32_t | timestamp |
| int32_t | altitude |
| int16_t | temperature |
This structure defines the mpl3115 data buffer in Altitude Mode.
Definition at line 80 of file mpl3115_drv.h.
| int32_t altitude |
Sensor pressure/altitude output: MS 16-bits are integer meters; LS 4-bits are fractional meters.
Definition at line 83 of file mpl3115_drv.h.
Referenced by main().
| int16_t temperature |
Sensor temperature output; 2's complement 12-bits justified to MSBs. MS 8-bits are integer degrees Celsius; LS 4-bits are fractional degrees Celsius.
Definition at line 85 of file mpl3115_drv.h.
Referenced by main().
| uint32_t timestamp |
Time stamp value in micro-seconds.
Definition at line 82 of file mpl3115_drv.h.