![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
This structure defines the mpl3115 data buffer in Pressure Mode. More...
#include <mpl3115_drv.h>

Data Fields | |
| uint32_t | timestamp |
| uint32_t | pressure |
| int16_t | temperature |
This structure defines the mpl3115 data buffer in Pressure Mode.
Definition at line 71 of file mpl3115_drv.h.
| uint32_t pressure |
Sensor pressure output: unsigned 20-bits justified to MSBs.
Definition at line 74 of file mpl3115_drv.h.
Referenced by main().
| int16_t temperature |
Sensor temperature output; 2's complement 12-bits justified to MSBs. MS 8-bits are integer degrees Celsius; LS 4-bits are fractional degrees Celsius.
Definition at line 75 of file mpl3115_drv.h.
Referenced by main().
| uint32_t timestamp |
Time stamp value in micro-seconds.
Definition at line 73 of file mpl3115_drv.h.
Referenced by main().