Files | |
| file | ble_constants.h |
Macros | |
| #define | gcBleDeviceAddressSize_c |
| #define | gBleBondIdentityHeaderSize_c |
| #define | gBleBondDataDynamicSize_c |
| #define | gBleBondDataStaticSize_c |
| #define | gBleBondDataDeviceInfoSize_c |
| #define | gBleBondDataDescriptorSize_c |
| #define | gcGapMaximumSavedCccds_c |
| #define | gBleBondDataSize_c |
| #define | gcGapMaxAuthorizationHandles_c |
| #define | gcGapMaxServiceSpecificSecurityRequirements_c |
| #define | gcBleLongUuidSize_c |
| #define | gcSmpMaxLtkSize_c |
| #define | gcSmpIrkSize_c |
| #define | gcSmpCsrkSize_c |
| #define | gcSmpMaxRandSize_c |
| #define | gcSmpOobSize_c |
| #define | gSmpLeScRandomValueSize_c |
| #define | gSmpLeScRandomConfirmValueSize_c |
| #define | gcGapMaxDeviceNameSize_c |
| #define | gcGapMaxAdvertisingDataLength_c |
| #define | gAttDefaultMtu_c |
| #define | gAttMaxMtu_c |
| #define | gcGattDbMaxPrepareWriteClients_c |
| #define | gHciTransportUartChannel_c |
| #define | gcReservedFlashSizeForCustomInformation_c |
| #define | gcGapControllerResolvingListSize_c |
| #define gcBleDeviceAddressSize_c |
Size of a BLE Device Address.
| #define gBleBondIdentityHeaderSize_c |
Size of bond data structures for a bonded device.
| #define gcGapMaximumSavedCccds_c |
Maximum number of CCCDs.
| #define gBleBondDataSize_c |
Bonding Data Size.
| #define gcGapMaxAuthorizationHandles_c |
Maximum number of attributes that require authorization.
| #define gcGapMaxServiceSpecificSecurityRequirements_c |
Maximum number of gapServiceSecurityRequirements_t structures that can be registered with Gap_RegisterDeviceSecurityRequirements()
| #define gcBleLongUuidSize_c |
Size of long UUIDs.
| #define gcSmpMaxLtkSize_c |
Maximum Long Term Key size in bytes.
| #define gcSmpIrkSize_c |
Identity Resolving Key size in bytes.
| #define gcSmpCsrkSize_c |
Connection Signature Resolving Key size in bytes.
| #define gcSmpMaxRandSize_c |
Maximum Rand size in bytes.
| #define gcSmpOobSize_c |
SMP OOB size in bytes.
| #define gSmpLeScRandomValueSize_c |
SMP LE Secure Connections Pairing Random size in bytes (BLE 4.2 only)
| #define gSmpLeScRandomConfirmValueSize_c |
SMP LE Secure Connections Pairing Confirm size in bytes (BLE 4.2 only)
| #define gcGapMaxDeviceNameSize_c |
Maximum device name size.
| #define gcGapMaxAdvertisingDataLength_c |
Maximum size of advertising and scan response data.
| #define gAttDefaultMtu_c |
Default value of the ATT_MTU.
| #define gAttMaxMtu_c |
Maximum possible value of the ATT_MTU for this device.
This is used during the MTU Exchange.
| #define gcGattDbMaxPrepareWriteClients_c |
Maximum number of simultaneous GATT Clients allowed to use Prepare Write Queues.
| #define gHciTransportUartChannel_c |
Channel the number of the UART hardware module (For example, if UART1 is used, this value should be 1).
| #define gcReservedFlashSizeForCustomInformation_c |
Number of bytes reserved for storing application-specific information about a device.
| #define gcGapControllerResolvingListSize_c |
Size of Controller's Resolving List (BLE 4.2 only).