Bluetooth Low Energy Host Stack  Rev. 4
API Reference Manual
GATT_DB - GATT Database Interface and Definitions

Overview


 

Files

file  gatt_database.h
 
file  gatt_db_app_interface.h
 

Data Structures

struct  gattDbAttribute_t
 

Macros

#define gGattDbInvalidHandleIndex_d
 
#define gGattDbInvalidHandle_d
 

Enumerations

enum  gattCharacteristicPropertiesBitFields_t {
  gGattCharPropNone_c, gGattCharPropBroadcast_c, gGattCharPropRead_c, gGattCharPropWriteWithoutRsp_c,
  gGattCharPropWrite_c, gGattCharPropNotify_c, gGattCharPropIndicate_c, gGattCharPropAuthSignedWrites_c,
  gGattCharPropExtendedProperties_c
}
 
enum  gattAttributePermissionsBitFields_t {
  gPermissionNone_c, gPermissionFlagReadable_c, gPermissionFlagReadWithEncryption_c, gPermissionFlagReadWithAuthentication_c,
  gPermissionFlagReadWithAuthorization_c, gPermissionFlagWritable_c, gPermissionFlagWriteWithEncryption_c, gPermissionFlagWriteWithAuthentication_c,
  gPermissionFlagWriteWithAuthorization_c
}
 
enum  gattDbAccessType_t { gAccessRead_c, gAccessWrite_c, gAccessNotify_c }
 

Functions

uint16_t GattDb_GetIndexOfHandle (uint16_t handle)
 
bleResult_t GattDb_Init ()
 
bleResult_t GattDb_WriteAttribute (uint16_t handle, uint16_t valueLength, uint8_t *aValue)
 
bleResult_t GattDb_ReadAttribute (uint16_t handle, uint16_t maxBytes, uint8_t *aOutValue, uint16_t *pOutValueLength)
 
bleResult_t GattDb_FindServiceHandle (uint16_t startHandle, bleUuidType_t serviceUuidType, bleUuid_t *pServiceUuid, uint16_t *pOutServiceHandle)
 
bleResult_t GattDb_FindCharValueHandleInService (uint16_t serviceHandle, bleUuidType_t characteristicUuidType, bleUuid_t *pCharacteristicUuid, uint16_t *pOutCharValueHandle)
 
bleResult_t GattDb_FindCccdHandleForCharValueHandle (uint16_t charValueHandle, uint16_t *pOutCccdHandle)
 
bleResult_t GattDb_FindDescriptorHandleForCharValueHandle (uint16_t charValueHandle, bleUuidType_t descriptorUuidType, bleUuid_t *pDescriptorUuid, uint16_t *pOutDescriptorHandle)
 

Variables

uint16_t gGattDbAttributeCount_c
 
gattDbAttribute_t * gattDatabase
 

Data Structure Documentation

◆ gattDbAttribute_t

struct gattDbAttribute_t

Attribute structure.

Data Fields
uint16_t handle The attribute handle - cannot be 0x0000.

The attribute handles need not be consecutive, but must be strictly increasing.

uint16_t permissions Attribute permissions as defined by the ATT.
uint32_t uuid The UUID should be read according to the gattDbAttribute_t.uuidType member: for 2-byte and 4-byte UUIDs, this contains the value of the UUID; for 16-byte UUIDs, this is a pointer to the allocated 16-byte array containing the UUID.
uint8_t * pValue A pointer to allocated value array.
uint16_t valueLength The size of the value array.
uint16_t uuidType: 2 Identifies the length of the UUID; values interpreted according to the bleUuidType_t enumeration.
uint16_t maxVariableValueLength: 10 The maximum length of the attribute value array; if this is set to 0, then the attribute's length is fixed and cannot be changed.

Macro Definition Documentation

◆ gGattDbInvalidHandleIndex_d

#define gGattDbInvalidHandleIndex_d

Special value returned by GattDb_GetIndexOfHandle to signal that an invalid attribute handle was given as parameter.

◆ gGattDbInvalidHandle_d

#define gGattDbInvalidHandle_d

Special value used to mark an invalid attribute handle.

Attribute handles are strictly positive.

Enumeration Type Documentation

◆ gattCharacteristicPropertiesBitFields_t

Bit fields for Characteristic properties.

Enumerator
gGattCharPropNone_c 

No Properties selected.

gGattCharPropBroadcast_c 

Characteristic can be broadcast.

gGattCharPropRead_c 

Characteristic can be read.

gGattCharPropWriteWithoutRsp_c 

Characteristic can be written without response.

gGattCharPropWrite_c 

Characteristic can be written with response.

gGattCharPropNotify_c 

Characteristic can be notified.

gGattCharPropIndicate_c 

Characteristic can be indicated.

gGattCharPropAuthSignedWrites_c 

Characteristic can be written with signed data.

gGattCharPropExtendedProperties_c 

Extended Characteristic properties.

◆ gattAttributePermissionsBitFields_t

Bit fields for attribute permissions.

Enumerator
gPermissionNone_c 

No permissions selected.

gPermissionFlagReadable_c 

Attribute can be read.

gPermissionFlagReadWithEncryption_c 

Attribute may be read only if link is encrypted.

gPermissionFlagReadWithAuthentication_c 

Attribute may be read only by authenticated peers.

gPermissionFlagReadWithAuthorization_c 

Attribute may be read only by authorized peers.

gPermissionFlagWritable_c 

Attribute can be written.

gPermissionFlagWriteWithEncryption_c 

Attribute may be written only if link is encrypted.

gPermissionFlagWriteWithAuthentication_c 

Attribute may be written only by authenticated peers.

gPermissionFlagWriteWithAuthorization_c 

Attribute may be written only by authorized peers.

◆ gattDbAccessType_t

Attribute access type.

Function Documentation

◆ GattDb_GetIndexOfHandle()

uint16_t GattDb_GetIndexOfHandle ( uint16_t  handle)


Returns the database index for a given attribute handle.

Parameters
[in]handleThe attribute handle.
Returns
The index of the given attribute in the database or gGattDbInvalidHandleIndex_d.

◆ GattDb_Init()

bleResult_t GattDb_Init ( )


Initializes the GATT database at runtime.

Remarks
This function should be called only once at device start-up. In the current stack implementation, it is called internally by Ble_HostInitialize.
This function executes synchronously.
Returns
gBleSuccess_c or error.

◆ GattDb_WriteAttribute()

bleResult_t GattDb_WriteAttribute ( uint16_t  handle,
uint16_t  valueLength,
uint8_t *  aValue 
)

Writes an attribute from the application level.

This function can be called by the application code to modify an attribute in the database. It should only be used by the application to modify a Characteristic's value based on the application logic (e.g., external sensor readings).

Parameters
[in]handleThe handle of the attribute to be written.
[in]valueLengthThe number of bytes to be written.
[in]aValueThe source buffer containing the value to be written.
Returns
gBleSuccess_c or error.
Remarks
This function executes synchronously.

◆ GattDb_ReadAttribute()

bleResult_t GattDb_ReadAttribute ( uint16_t  handle,
uint16_t  maxBytes,
uint8_t *  aOutValue,
uint16_t *  pOutValueLength 
)

Reads an attribute from the application level.

This function can be called by the application code to read an attribute in the database.

Parameters
[in]handleThe handle of the attribute to be read.
[in]maxBytesThe maximum number of bytes to be received.
[out]aOutValueThe pre-allocated buffer ready to receive the bytes.
[out]pOutValueLengthThe actual number of bytes received.
Returns
gBleSuccess_c or error.
Remarks
This function executes synchronously.

◆ GattDb_FindServiceHandle()

bleResult_t GattDb_FindServiceHandle ( uint16_t  startHandle,
bleUuidType_t  serviceUuidType,
bleUuid_t *  pServiceUuid,
uint16_t *  pOutServiceHandle 
)

Finds the handle of a Service Declaration with a given UUID inside the database.

Parameters
[in]startHandleThe handle to start the search. Should be 0x0001 on the first call.
[in]serviceUuidTypeService UUID type.
[in]pServiceUuidService UUID.
[out]pOutServiceHandlePointer to the service declaration handle to be written.
Returns
gBleSuccess_c or error.
Return values
gBleSuccess_cService Declaration found, handle written in pOutCharValueHandle.
gGattDbInvalidHandle_cInvalid Start Handle.
gGattDbServiceNotFound_cService with given UUID not found.
Remarks
This function executes synchronously.
The startHandle should be set to 0x0001 when this function is called for the first time. If multiple Services with the same UUID are expected, then after the first successful call the function may be called again with the startHandle equal to the found service handle plus one.

◆ GattDb_FindCharValueHandleInService()

bleResult_t GattDb_FindCharValueHandleInService ( uint16_t  serviceHandle,
bleUuidType_t  characteristicUuidType,
bleUuid_t *  pCharacteristicUuid,
uint16_t *  pOutCharValueHandle 
)

Finds the handle of a Characteristic Value with a given UUID inside a Service.

The Service is input by its declaration handle.

Parameters
[in]serviceHandleThe handle of the Service declaration.
[in]characteristicUuidTypeCharacteristic UUID type.
[in]pCharacteristicUuidCharacteristic UUID.
[out]pOutCharValueHandlePointer to the characteristic value handle to be written.
Returns
gBleSuccess_c or error.
Return values
gBleSuccess_cCharacteristic Value found, handle written in pOutCharValueHandle.
gGattDbInvalidHandle_cHandle not found or not a Service declaration.
gGattDbCharacteristicNotFound_cCharacteristic Value with given UUID not found.
Remarks
This function executes synchronously.

◆ GattDb_FindCccdHandleForCharValueHandle()

bleResult_t GattDb_FindCccdHandleForCharValueHandle ( uint16_t  charValueHandle,
uint16_t *  pOutCccdHandle 
)

Finds the handle of a Characteristic's CCCD given the Characteristic's Value handle.

Parameters
[in]charValueHandleThe handle of the Service declaration.
[out]pOutCccdHandlePointer to the CCCD handle to be written.
Returns
gBleSuccess_c or error.
Return values
gBleSuccess_cCCCD found, handle written in pOutCccdHandle.
gGattDbInvalidHandle_cInvalid Characteristic Value handle.
gGattDbCccdNotFound_cCCCD not found for this Characteristic.
Remarks
This function executes synchronously.

◆ GattDb_FindDescriptorHandleForCharValueHandle()

bleResult_t GattDb_FindDescriptorHandleForCharValueHandle ( uint16_t  charValueHandle,
bleUuidType_t  descriptorUuidType,
bleUuid_t *  pDescriptorUuid,
uint16_t *  pOutDescriptorHandle 
)

Finds the handle of a Characteristic Descriptor given the Characteristic's Value handle and Descriptor's UUID.

Parameters
[in]charValueHandleThe handle of the Service declaration.
[in]descriptorUuidTypeDescriptor's UUID type.
[in]pDescriptorUuidDescriptor's UUID.
[out]pOutDescriptorHandlePointer to the Descriptor handle to be written.
Returns
gBleSuccess_c or error.
Return values
gBleSuccess_cDescriptor found, handle written in pOutDescriptorHandle.
gGattDbInvalidHandle_cInvalid Characteristic Value handle.
gGattDbDescriptorNotFound_cDescriptor not found for this Characteristic.
Remarks
This function executes synchronously.

Variable Documentation

◆ gGattDbAttributeCount_c

uint16_t gGattDbAttributeCount_c

The number of attributes in the GATT Database.

◆ gattDatabase

gattDbAttribute_t* gattDatabase

Reference to the GATT database.