42 #define SENSOR_MAX_REGISTER_COUNT 128     45 #define __END_WRITE_DATA__            \    47         .writeTo = 0xFFFF, .value = 0 \    51 #define __END_READ_DATA__                 \    53         .readFrom = 0xFFFF, .numBytes = 0 \    57 #define __END_WRITE_CMD__                \    59         .writeTo = 0xFFFF, .numBytes = 0 \   109 #endif //_SENSOR_DRV_H 
This structure defines the device specific info required by register I/O. 
 
This structure defines the Write command List. 
 
enum EWriteFlags EWriteFlags_t
 
This structure defines the Block command List. 
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
This structure defines the Read command List. 
 
const uint8_t * pWriteBuffer
 
registeridlefunction_t idleFunction