15 #ifndef __SENSOR_IO_I2C_H 16 #define __SENSOR_IO_I2C_H 20 #include "Driver_I2C.h" 38 uint16_t slaveAddress,
53 uint16_t slaveAddress,
69 uint16_t slaveAddress,
This structure defines the device specific info required by register I/O.
This structure defines the Write command List.
This structure defines the Block command List.
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream.
The register_io_i2c.h file declares low-level interface functions for reading and writing sensor regi...
int32_t Sensor_I2C_BlockWrite(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registercommandlist_t *pCommandList, uint8_t error_mask)
Write commands to a sensor.
int32_t Sensor_I2C_Write(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerwritelist_t *pRegWriteList)
Write register data to a sensor.
This structure defines the Read command List.
int32_t Sensor_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerreadlist_t *pReadList, uint8_t *pOutBuffer)
Read register data from a sensor.