![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The frdm_stbc_b3115_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-kl27z and frmd-stbc-b3115 shield. More...

Go to the source code of this file.
Macros | |
| #define | SHIELD_NAME "FRDMSTBC-B3115" |
| #define | FXPQ3115_I2C_ADDR 0x60 |
| #define | FXPQ3115_INT1 D5 |
| #define | FXPQ3115_INT2 D2 |
The frdm_stbc_b3115_shield.h file declares mapping of the Kinetis Device peripherals to the frmd-kl27z and frmd-stbc-b3115 shield.
Definition in file frdm_stbc_b3115_shield.h.
| #define FXPQ3115_I2C_ADDR 0x60 |
Definition at line 22 of file frdm_stbc_b3115_shield.h.
| #define FXPQ3115_INT1 D5 |
Definition at line 23 of file frdm_stbc_b3115_shield.h.
Referenced by main().
| #define FXPQ3115_INT2 D2 |
Definition at line 24 of file frdm_stbc_b3115_shield.h.
| #define SHIELD_NAME "FRDMSTBC-B3115" |
Definition at line 19 of file frdm_stbc_b3115_shield.h.