![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|

Go to the source code of this file.
Macros | |
| #define | SHIELD_NAME "FRDM-STBI-DP300x" |
| #define | DBAP_I2C_ADDR 0x60 |
| #define | DIFF_P_INT1 D5 |
| #define | DIFF_P_INT2 D2 |
| #define | DIFF_P_CS D10 |
| #define DBAP_I2C_ADDR 0x60 |
Definition at line 21 of file frdm-stba-pd7250_shield.h.
| #define DIFF_P_CS D10 |
Definition at line 24 of file frdm-stba-pd7250_shield.h.
| #define DIFF_P_INT1 D5 |
Definition at line 22 of file frdm-stba-pd7250_shield.h.
Referenced by main().
| #define DIFF_P_INT2 D2 |
Definition at line 23 of file frdm-stba-pd7250_shield.h.
| #define SHIELD_NAME "FRDM-STBI-DP300x" |
Definition at line 18 of file frdm-stba-pd7250_shield.h.