![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|

Go to the source code of this file.
Macros | |
| #define | SHIELD_NAME "FRDM-STBC-DIFF-P" |
| #define | NPS3000VV_PRESSURE_DIV_FACTOR (8) |
| #define | NPS3001DV_PRESSURE_DIV_FACTOR (8) |
| #define | NPS3002VV_PRESSURE_DIV_FACTOR (4) |
| #define | NPS3005DV_PRESSURE_DIV_FACTOR (4) |
| #define | DIFF_P_I2C_ADDR 0x60 |
| #define | DIFF_P_INT1 D5 |
| #define | DIFF_P_INT2 D2 |
| #define | DIFF_P_CS D10 |
| #define DIFF_P_CS D10 |
Definition at line 30 of file frdm-stbc-diffp_shield.h.
| #define DIFF_P_I2C_ADDR 0x60 |
Definition at line 27 of file frdm-stbc-diffp_shield.h.
| #define DIFF_P_INT1 D5 |
Definition at line 28 of file frdm-stbc-diffp_shield.h.
| #define DIFF_P_INT2 D2 |
Definition at line 29 of file frdm-stbc-diffp_shield.h.
| #define NPS3000VV_PRESSURE_DIV_FACTOR (8) |
Definition at line 21 of file frdm-stbc-diffp_shield.h.
| #define NPS3001DV_PRESSURE_DIV_FACTOR (8) |
Definition at line 22 of file frdm-stbc-diffp_shield.h.
| #define NPS3002VV_PRESSURE_DIV_FACTOR (4) |
Definition at line 23 of file frdm-stbc-diffp_shield.h.
| #define NPS3005DV_PRESSURE_DIV_FACTOR (4) |
Definition at line 24 of file frdm-stbc-diffp_shield.h.
| #define SHIELD_NAME "FRDM-STBC-DIFF-P" |
Definition at line 18 of file frdm-stbc-diffp_shield.h.