19 .irq = GPIO1_Combined_0_15_IRQn,
24 .irq = GPIO1_Combined_0_15_IRQn,
31 .irq = GPIO1_Combined_16_31_IRQn,
36 .irq = GPIO1_Combined_16_31_IRQn,
43 .irq = GPIO3_Combined_0_15_IRQn,
48 .irq = GPIO3_Combined_0_15_IRQn,
53 .irq = GPIO3_Combined_0_15_IRQn,
58 .irq = GPIO3_Combined_0_15_IRQn,
65 .irq = GPIO1_Combined_16_31_IRQn,
70 .irq = GPIO1_Combined_16_31_IRQn,
77 .irq = GPIO1_Combined_16_31_IRQn,
82 .irq = GPIO1_Combined_16_31_IRQn,
87 .irq = GPIO1_Combined_16_31_IRQn,
92 .irq = GPIO1_Combined_16_31_IRQn,
97 .irq = GPIO1_Combined_0_15_IRQn,
102 .irq = GPIO1_Combined_16_31_IRQn,
107 .irq = GPIO1_Combined_0_15_IRQn,
112 .irq = GPIO1_Combined_0_15_IRQn,
117 .irq = GPIO1_Combined_16_31_IRQn,
122 .irq = GPIO1_Combined_16_31_IRQn,
127 .irq = GPIO1_Combined_0_15_IRQn,
132 .irq = GPIO1_Combined_0_15_IRQn,
140 .irq = GPIO1_Combined_0_15_IRQn,
145 .irq = GPIO1_Combined_0_15_IRQn,
150 .irq = GPIO1_Combined_0_15_IRQn,
157 .irq = GPIO1_Combined_0_15_IRQn,
162 .irq = GPIO1_Combined_0_15_IRQn,
169 static void stop(
void)
171 SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
184 CLOCK_SetMode(kCLOCK_ModeWait);
187 return kStatus_Success;
199 CLOCK_SetMode(kCLOCK_ModeWait);
202 return kStatus_Success;
214 return CLOCK_GetFreq((clock_name_t) kCLOCK_Lpuart1);
226 return CLOCK_GetFreq((clock_name_t) kCLOCK_Lpi2c1);
238 return CLOCK_GetFreq((clock_name_t) kCLOCK_Lpspi1);
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
uint32_t LPI2C1_GetFreq(void)
Determines the Clock Frequency feature.
gpioHandleiMXSDK_t RED_LED
uint32_t LPUART1_GetFreq(void)
Determines the Clock Frequency feature.
gpioHandleiMXSDK_t BLUE_LED
The GPIO pin handle for i.MX SDK.
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
gpioHandleiMXSDK_t GREEN_LED
uint32_t LPSPI1_GetFreq(void)
Determines the Clock Frequency feature.
The evkbimxrt1050.h file defines GPIO pin mappings for evkbimxrt1050 board.