![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The evkmimxrt1064.c file defines GPIO pins and I2C CMSIS utilities for evkmimxrt1064 board. More...
#include "evkmimxrt1064.h"
Go to the source code of this file.
Functions | |
| status_t | SMC_SetPowerModeWait (void *arg) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *arg) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
| uint32_t | LPUART1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | LPI2C1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | LPSPI1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
The evkmimxrt1064.c file defines GPIO pins and I2C CMSIS utilities for evkmimxrt1064 board.
Definition in file evkmimxrt1064.c.
| uint32_t LPI2C1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 224 of file evkmimxrt1064.c.
| uint32_t LPSPI1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 236 of file evkmimxrt1064.c.
| uint32_t LPUART1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 212 of file evkmimxrt1064.c.
| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 197 of file evkmimxrt1064.c.
| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 182 of file evkmimxrt1064.c.
Definition at line 74 of file evkmimxrt1064.c.
Definition at line 79 of file evkmimxrt1064.c.
Definition at line 84 of file evkmimxrt1064.c.
Definition at line 89 of file evkmimxrt1064.c.
Definition at line 33 of file evkmimxrt1064.c.
Definition at line 28 of file evkmimxrt1064.c.
| gpioHandleiMXSDK_t BLUE_LED |
Definition at line 147 of file evkmimxrt1064.c.
Definition at line 62 of file evkmimxrt1064.c.
Definition at line 67 of file evkmimxrt1064.c.
Definition at line 55 of file evkmimxrt1064.c.
Definition at line 50 of file evkmimxrt1064.c.
Definition at line 45 of file evkmimxrt1064.c.
Definition at line 40 of file evkmimxrt1064.c.
Definition at line 21 of file evkmimxrt1064.c.
Definition at line 16 of file evkmimxrt1064.c.
Definition at line 94 of file evkmimxrt1064.c.
Definition at line 99 of file evkmimxrt1064.c.
Definition at line 104 of file evkmimxrt1064.c.
Definition at line 109 of file evkmimxrt1064.c.
Definition at line 114 of file evkmimxrt1064.c.
Definition at line 119 of file evkmimxrt1064.c.
Definition at line 124 of file evkmimxrt1064.c.
Definition at line 129 of file evkmimxrt1064.c.
| gpioHandleiMXSDK_t GREEN_LED |
Definition at line 142 of file evkmimxrt1064.c.
| gpioHandleiMXSDK_t INT1 |
Definition at line 154 of file evkmimxrt1064.c.
| gpioHandleiMXSDK_t INT2 |
Definition at line 159 of file evkmimxrt1064.c.
| gpioHandleiMXSDK_t RED_LED |
Definition at line 137 of file evkmimxrt1064.c.