18 #include "Driver_I2C.h"    19 #include "Driver_SPI.h" int8_t FXLS8471Q_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MAG3110_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MMA8451_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MPL3115_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXLS8972_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MMA8652_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXLS8972_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
An instance of PhysicalSensor structure type should be allocated for each physical sensors (combo dev...
 
int8_t MMA8652_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXLS8952_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXLS8962_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXOS8700_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MAG3110_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
The top level fusion structure. 
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
int8_t FXLS8972_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int32_t ARM_systick_elapsed_ticks(int32_t start_ticks)
 
int8_t FXAS21002_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MMA8451_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXLS8471Q_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MPL3115_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
void ARM_systick_start_ticks(int32_t *pstart)
 
int8_t MMA8652_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MMA8451_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXLS8962_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXOS8700_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXAS21002_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXLS8962_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXLS8952_Init(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
void ARM_systick_enable(void)
 
int8_t FXLS8952_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
void ARM_systick_delay_ms(uint32_t iSystemCoreClock, uint32_t delay_ms)
 
int8_t FXLS8471Q_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MPL3115_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXOS8700_Idle(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t MAG3110_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)
 
int8_t FXAS21002_Read(struct PhysicalSensor *sensor, SensorFusionGlobals *sfg)