ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXAS21002_DR_STATUS_t Union Reference

#include <fxas21002.h>

Collaboration diagram for FXAS21002_DR_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xdr: 1
 
   uint8_t   ydr: 1
 
   uint8_t   zdr: 1
 
   uint8_t   zyxdr: 1
 
   uint8_t   xow: 1
 
   uint8_t   yow: 1
 
   uint8_t   zow: 1
 
   uint8_t   zyxow: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 125 of file fxas21002.h.

Field Documentation

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 144 of file fxas21002.h.

◆ xdr

uint8_t xdr

Definition at line 127 of file fxas21002.h.

◆ xow

uint8_t xow

Definition at line 135 of file fxas21002.h.

◆ ydr

uint8_t ydr

Definition at line 129 of file fxas21002.h.

◆ yow

uint8_t yow

Definition at line 137 of file fxas21002.h.

◆ zdr

uint8_t zdr

Definition at line 131 of file fxas21002.h.

◆ zow

uint8_t zow

Definition at line 139 of file fxas21002.h.

◆ zyxdr

uint8_t zyxdr

Definition at line 133 of file fxas21002.h.

◆ zyxow

uint8_t zyxow

Definition at line 141 of file fxas21002.h.


The documentation for this union was generated from the following file: