ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXAS21002_INT_SRC_FLAG_t Union Reference

#include <fxas21002.h>

Collaboration diagram for FXAS21002_INT_SRC_FLAG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   src_drdy: 1
 
   uint8_t   src_rt: 1
 
   uint8_t   src_fifo: 1
 
   uint8_t   bootend: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 329 of file fxas21002.h.

Field Documentation

◆ b

struct { ... } b

◆ bootend

uint8_t bootend

Definition at line 337 of file fxas21002.h.

◆ src_drdy

uint8_t src_drdy

Definition at line 331 of file fxas21002.h.

◆ src_fifo

uint8_t src_fifo

Definition at line 335 of file fxas21002.h.

◆ src_rt

uint8_t src_rt

Definition at line 333 of file fxas21002.h.

◆ w

uint8_t w

Definition at line 340 of file fxas21002.h.


The documentation for this union was generated from the following file: