ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXAS21002_CTRL_REG0_t Union Reference

#include <fxas21002.h>

Collaboration diagram for FXAS21002_CTRL_REG0_t:
Collaboration graph

Data Fields

struct {
   uint8_t   fs: 2
 
   uint8_t   hpf_en: 1
 
   uint8_t   sel: 2
 
   uint8_t   spiw: 1
 
   uint8_t   bw: 2
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 412 of file fxas21002.h.

Field Documentation

◆ b

struct { ... } b

◆ bw

uint8_t bw

Definition at line 425 of file fxas21002.h.

◆ fs

uint8_t fs

Definition at line 414 of file fxas21002.h.

◆ hpf_en

uint8_t hpf_en

Definition at line 416 of file fxas21002.h.

◆ sel

uint8_t sel

Definition at line 421 of file fxas21002.h.

◆ spiw

uint8_t spiw

Definition at line 423 of file fxas21002.h.

◆ w

uint8_t w

Definition at line 428 of file fxas21002.h.


The documentation for this union was generated from the following file: