ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXAS21002_RT_CFG_t Union Reference

#include <fxas21002.h>

Collaboration diagram for FXAS21002_RT_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xtefe: 1
 
   uint8_t   ytefe: 1
 
   uint8_t   ztefe: 1
 
   uint8_t   ele: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 477 of file fxas21002.h.

Field Documentation

◆ b

struct { ... } b

◆ ele

uint8_t ele

Definition at line 485 of file fxas21002.h.

◆ w

uint8_t w

Definition at line 488 of file fxas21002.h.

◆ xtefe

uint8_t xtefe

Definition at line 479 of file fxas21002.h.

◆ ytefe

uint8_t ytefe

Definition at line 481 of file fxas21002.h.

◆ ztefe

uint8_t ztefe

Definition at line 483 of file fxas21002.h.


The documentation for this union was generated from the following file: