ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXAS21002_RT_SRC_t Union Reference

#include <fxas21002.h>

Collaboration diagram for FXAS21002_RT_SRC_t:
Collaboration graph

Data Fields

struct {
   uint8_t   x_rt_pol: 1
 
   uint8_t   xrt: 1
 
   uint8_t   y_rt_pol: 1
 
   uint8_t   yrt: 1
 
   uint8_t   z_rt_pol: 1
 
   uint8_t   zrt: 1
 
   uint8_t   ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 529 of file fxas21002.h.

Field Documentation

◆ b

struct { ... } b

◆ ea

uint8_t ea

Definition at line 543 of file fxas21002.h.

◆ w

uint8_t w

Definition at line 546 of file fxas21002.h.

◆ x_rt_pol

uint8_t x_rt_pol

Definition at line 531 of file fxas21002.h.

◆ xrt

uint8_t xrt

Definition at line 533 of file fxas21002.h.

◆ y_rt_pol

uint8_t y_rt_pol

Definition at line 535 of file fxas21002.h.

◆ yrt

uint8_t yrt

Definition at line 537 of file fxas21002.h.

◆ z_rt_pol

uint8_t z_rt_pol

Definition at line 539 of file fxas21002.h.

◆ zrt

uint8_t zrt

Definition at line 541 of file fxas21002.h.


The documentation for this union was generated from the following file: