ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXAS21002_CTRL_REG2_t Union Reference

#include <fxas21002.h>

Collaboration diagram for FXAS21002_CTRL_REG2_t:
Collaboration graph

Data Fields

struct {
   uint8_t   pp_od: 1
 
   uint8_t   ipol: 1
 
   uint8_t   int_en_drdy: 1
 
   uint8_t   int_cfg_drdy: 1
 
   uint8_t   int_en_rt: 1
 
   uint8_t   int_cfg_rt: 1
 
   uint8_t   int_en_fifo: 1
 
   uint8_t   int_cfg_fifo: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 725 of file fxas21002.h.

Field Documentation

◆ b

struct { ... } b

◆ int_cfg_drdy

uint8_t int_cfg_drdy

Definition at line 733 of file fxas21002.h.

◆ int_cfg_fifo

uint8_t int_cfg_fifo

Definition at line 741 of file fxas21002.h.

◆ int_cfg_rt

uint8_t int_cfg_rt

Definition at line 737 of file fxas21002.h.

◆ int_en_drdy

uint8_t int_en_drdy

Definition at line 731 of file fxas21002.h.

◆ int_en_fifo

uint8_t int_en_fifo

Definition at line 739 of file fxas21002.h.

◆ int_en_rt

uint8_t int_en_rt

Definition at line 735 of file fxas21002.h.

◆ ipol

uint8_t ipol

Definition at line 729 of file fxas21002.h.

◆ pp_od

uint8_t pp_od

Definition at line 727 of file fxas21002.h.

◆ w

uint8_t w

Definition at line 744 of file fxas21002.h.


The documentation for this union was generated from the following file: