ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXAS21002_CTRL_REG3_t Union Reference

#include <fxas21002.h>

Collaboration diagram for FXAS21002_CTRL_REG3_t:
Collaboration graph

Data Fields

struct {
   uint8_t   fs_double: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   extctrlen: 1
 
   uint8_t   wraptoone: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 805 of file fxas21002.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 810 of file fxas21002.h.

◆ b

struct { ... } b

◆ extctrlen

uint8_t extctrlen

Definition at line 811 of file fxas21002.h.

◆ fs_double

uint8_t fs_double

Definition at line 807 of file fxas21002.h.

◆ w

uint8_t w

Definition at line 816 of file fxas21002.h.

◆ wraptoone

uint8_t wraptoone

Definition at line 813 of file fxas21002.h.


The documentation for this union was generated from the following file: