ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_INT_STATUS_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_INT_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   src_boot: 1
 
   uint8_t   src_aslp: 1
 
   uint8_t   src_orient: 1
 
   uint8_t   src_sdcd_wt: 1
 
   uint8_t   src_sdcd_ot: 1
 
   uint8_t   src_buf: 1
 
   uint8_t   src_ovf: 1
 
   uint8_t   src_drdy: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 99 of file fxls8962.h.

Field Documentation

◆ b

struct { ... } b

◆ src_aslp

uint8_t src_aslp

Definition at line 105 of file fxls8962.h.

◆ src_boot

uint8_t src_boot

Definition at line 103 of file fxls8962.h.

◆ src_buf

uint8_t src_buf

Definition at line 113 of file fxls8962.h.

◆ src_drdy

uint8_t src_drdy

Definition at line 117 of file fxls8962.h.

◆ src_orient

uint8_t src_orient

Definition at line 107 of file fxls8962.h.

◆ src_ovf

uint8_t src_ovf

Definition at line 115 of file fxls8962.h.

◆ src_sdcd_ot

uint8_t src_sdcd_ot

Definition at line 111 of file fxls8962.h.

◆ src_sdcd_wt

uint8_t src_sdcd_wt

Definition at line 109 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 120 of file fxls8962.h.


The documentation for this union was generated from the following file: