ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_PROD_REV_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_PROD_REV_t:
Collaboration graph

Data Fields

struct {
   uint8_t   prod_rev_min: 4
 
   uint8_t   prod_rev_maj: 4
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 316 of file fxls8962.h.

Field Documentation

◆ b

struct { ... } b

◆ prod_rev_maj

uint8_t prod_rev_maj

Definition at line 323 of file fxls8962.h.

◆ prod_rev_min

uint8_t prod_rev_min

Definition at line 320 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 327 of file fxls8962.h.


The documentation for this union was generated from the following file: