ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_SENS_CONFIG2_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_SENS_CONFIG2_t:
Collaboration graph

Data Fields

struct {
   uint8_t   f_read: 1
 
   uint8_t   anic_temp: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   le_be: 1
 
   uint8_t   sleep_pm: 2
 
   uint8_t   wake_pm: 2
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 471 of file fxls8962.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 479 of file fxls8962.h.

◆ anic_temp

uint8_t anic_temp

Definition at line 477 of file fxls8962.h.

◆ b

struct { ... } b

◆ f_read

uint8_t f_read

Definition at line 475 of file fxls8962.h.

◆ le_be

uint8_t le_be

Definition at line 480 of file fxls8962.h.

◆ sleep_pm

uint8_t sleep_pm

Definition at line 482 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 487 of file fxls8962.h.

◆ wake_pm

uint8_t wake_pm

Definition at line 484 of file fxls8962.h.


The documentation for this union was generated from the following file: