ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_SENS_CONFIG5_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_SENS_CONFIG5_t:
Collaboration graph

Data Fields

struct {
   uint8_t   hibernate_en: 1
 
   uint8_t   z_dis: 1
 
   uint8_t   y_dis: 1
 
   uint8_t   x_dis: 1
 
   uint8_t   vecm_en: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 690 of file fxls8962.h.

Field Documentation

◆ b

struct { ... } b

◆ hibernate_en

uint8_t hibernate_en

Definition at line 694 of file fxls8962.h.

◆ vecm_en

uint8_t vecm_en

Definition at line 702 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 705 of file fxls8962.h.

◆ x_dis

uint8_t x_dis

Definition at line 700 of file fxls8962.h.

◆ y_dis

uint8_t y_dis

Definition at line 698 of file fxls8962.h.

◆ z_dis

uint8_t z_dis

Definition at line 696 of file fxls8962.h.


The documentation for this union was generated from the following file: